<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2</title>
    <link>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1267676#M8450</link>
    <description>&lt;DIV class="gmail_default"&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;We have created custom boards using PN7362 RFID Controller. It is understood from the Quick Start Manual, UM10883, Section 6.9 The EEPROM has to be updated first before using any NXP Examples. The flashing of eeprom bin file is failing for me with error attached.&lt;/P&gt;&lt;P&gt;On the same side, Flash Programming works fine. Output Attached.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;</description>
    <pubDate>Sun, 25 Apr 2021 17:05:10 GMT</pubDate>
    <dc:creator>kashyap_gada</dc:creator>
    <dc:date>2021-04-25T17:05:10Z</dc:date>
    <item>
      <title>PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1267676#M8450</link>
      <description>&lt;DIV class="gmail_default"&gt;&lt;P&gt;Dear Sir,&lt;/P&gt;&lt;P&gt;We have created custom boards using PN7362 RFID Controller. It is understood from the Quick Start Manual, UM10883, Section 6.9 The EEPROM has to be updated first before using any NXP Examples. The flashing of eeprom bin file is failing for me with error attached.&lt;/P&gt;&lt;P&gt;On the same side, Flash Programming works fine. Output Attached.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Sun, 25 Apr 2021 17:05:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1267676#M8450</guid>
      <dc:creator>kashyap_gada</dc:creator>
      <dc:date>2021-04-25T17:05:10Z</dc:date>
    </item>
    <item>
      <title>Re: PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1268671#M8461</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/134279"&gt;@kashyap_gada&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is it possible to provide a snapshot to show how you configure the programming? As I know, the base address should be 0x201200 for EEPROM program.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for your patience!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 07:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1268671#M8461</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-04-27T07:54:00Z</dc:date>
    </item>
    <item>
      <title>Re: PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2</title>
      <link>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1268981#M8467</link>
      <description>&lt;P&gt;Dear Kan,&lt;/P&gt;&lt;P&gt;Thank for your reply.&lt;/P&gt;&lt;P&gt;I was following UM10883, but I didn't double check the EEPROM Address. I corrected the address and then program ran normally.&lt;/P&gt;&lt;P&gt;Thank you for your prompt reply!!!&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 27 Apr 2021 14:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7362-Custom-Board-EEPROM-Program-using-MCUXpresso-LPC-LINK2/m-p/1268981#M8467</guid>
      <dc:creator>kashyap_gada</dc:creator>
      <dc:date>2021-04-27T14:11:38Z</dc:date>
    </item>
  </channel>
</rss>