<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN5180 Evaluation Board Setup in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN5180-Evaluation-Board-Setup/m-p/1261534#M8426</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I bought a&amp;nbsp;&lt;SPAN&gt;PN5180 Evaluation board, and from the quick start guide I am trying to setup the board.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the directions in section 3.2.3 (option 2) it says replace the file on the board with an updated bin file. I managed to do that and the device restarts, but afterwards I still cannot connect to NFC Cockpit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have installed the drivers that came in the VCOM folder. But when I check device manager it is still saying it is a USB Serial device (in fact its saying it is 2 devices for some reason).&lt;/P&gt;&lt;P&gt;Is there an additional driver I am missing? I also tried to connect to MCUXpresso but I couldn't connect to that either.&lt;/P&gt;&lt;P&gt;Thank you for any assistance that can be provided&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;</description>
    <pubDate>Tue, 13 Apr 2021 22:03:27 GMT</pubDate>
    <dc:creator>BPJC</dc:creator>
    <dc:date>2021-04-13T22:03:27Z</dc:date>
    <item>
      <title>PN5180 Evaluation Board Setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Evaluation-Board-Setup/m-p/1261534#M8426</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I bought a&amp;nbsp;&lt;SPAN&gt;PN5180 Evaluation board, and from the quick start guide I am trying to setup the board.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the directions in section 3.2.3 (option 2) it says replace the file on the board with an updated bin file. I managed to do that and the device restarts, but afterwards I still cannot connect to NFC Cockpit.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I have installed the drivers that came in the VCOM folder. But when I check device manager it is still saying it is a USB Serial device (in fact its saying it is 2 devices for some reason).&lt;/P&gt;&lt;P&gt;Is there an additional driver I am missing? I also tried to connect to MCUXpresso but I couldn't connect to that either.&lt;/P&gt;&lt;P&gt;Thank you for any assistance that can be provided&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;</description>
      <pubDate>Tue, 13 Apr 2021 22:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Evaluation-Board-Setup/m-p/1261534#M8426</guid>
      <dc:creator>BPJC</dc:creator>
      <dc:date>2021-04-13T22:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Evaluation Board Setup</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Evaluation-Board-Setup/m-p/1261615#M8428</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Did you flash firmware after you run the library if you want to connect the board with cockpit? Please refer to the link for the detail information.&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://www.nxp.com.cn/docs/en/user-guide/UM10954.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/user-guide/UM10954.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Or in order to better service for you would you please provide the steps for your question?&lt;/P&gt;
&lt;P&gt;Hope it help you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 02:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Evaluation-Board-Setup/m-p/1261615#M8428</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-04-14T02:24:17Z</dc:date>
    </item>
  </channel>
</rss>