<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックiOS support  for Originality Signature reading and verification</title>
    <link>https://community.nxp.com/t5/NFC/iOS-support-for-Originality-Signature-reading-and-verification/m-p/1254919#M8372</link>
    <description>&lt;P&gt;Does iOS support Originality Signature reading in NTAG21x ICs ? if there is no direct command to do that, are there any methods to execute custom commands? I saw that iOS 13 supports custom commands for NFC type -v tags. Does it support custom commands for NFC type 2 tags (ISO14443) as well?&lt;/P&gt;</description>
    <pubDate>Wed, 31 Mar 2021 10:45:08 GMT</pubDate>
    <dc:creator>HP009</dc:creator>
    <dc:date>2021-03-31T10:45:08Z</dc:date>
    <item>
      <title>iOS support  for Originality Signature reading and verification</title>
      <link>https://community.nxp.com/t5/NFC/iOS-support-for-Originality-Signature-reading-and-verification/m-p/1254919#M8372</link>
      <description>&lt;P&gt;Does iOS support Originality Signature reading in NTAG21x ICs ? if there is no direct command to do that, are there any methods to execute custom commands? I saw that iOS 13 supports custom commands for NFC type -v tags. Does it support custom commands for NFC type 2 tags (ISO14443) as well?&lt;/P&gt;</description>
      <pubDate>Wed, 31 Mar 2021 10:45:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/iOS-support-for-Originality-Signature-reading-and-verification/m-p/1254919#M8372</guid>
      <dc:creator>HP009</dc:creator>
      <dc:date>2021-03-31T10:45:08Z</dc:date>
    </item>
    <item>
      <title>Re: iOS support  for Originality Signature reading and verification</title>
      <link>https://community.nxp.com/t5/NFC/iOS-support-for-Originality-Signature-reading-and-verification/m-p/1256410#M8383</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181420"&gt;@HP009&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Actually it is an implementation topic on application level, just as other commands implementation in an iOS App such as NTAG I2C Demo App, please kindly refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/NFC-Knowledge-Base/NTAG-I2C-Demo-iOS-source-code-sharing/ta-p/1225337?search-action-id=34167346673&amp;amp;search-result-uid=1225337" target="_blank"&gt;https://community.nxp.com/t5/NFC-Knowledge-Base/NTAG-I2C-Demo-iOS-source-code-sharing/ta-p/1225337?search-action-id=34167346673&amp;amp;search-result-uid=1225337&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Sat, 03 Apr 2021 02:42:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/iOS-support-for-Originality-Signature-reading-and-verification/m-p/1256410#M8383</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2021-04-03T02:42:56Z</dc:date>
    </item>
  </channel>
</rss>