<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Fastest encoder IC in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607405#M831</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the answer. Now the difference between the two IC become clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll buy a PN532 Arduino Shield and run some tests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;&lt;P&gt;Fernando Coelho&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Dec 2016 12:56:32 GMT</pubDate>
    <dc:creator>fernandohcoelho</dc:creator>
    <dc:date>2016-12-15T12:56:32Z</dc:date>
    <item>
      <title>Fastest encoder IC</title>
      <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607400#M826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with a arduino NFC shield, with a NXP RC522 chip. With my program, I'm getting this timming:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Discover tag: 25ms&lt;/P&gt;&lt;P&gt;Write mem sector: 10ms&lt;/P&gt;&lt;P&gt;Halt tag: 25ms&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question: Can I bring this values down with another NXP IC? Or this values are a technology limitation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I can do it faster, which IC must I use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!!&lt;/P&gt;&lt;P&gt;Fernando Coelho&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 12:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607400#M826</guid>
      <dc:creator>fernandohcoelho</dc:creator>
      <dc:date>2016-12-13T12:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: Fastest encoder IC</title>
      <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607401#M827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="291305" data-username="fernandohcoelho" href="https://community.nxp.com/people/fernandohcoelho"&gt;Fernando&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; The speed is not releated to reader IC, it is determined by 4 factors:&lt;/P&gt;&lt;P&gt;(1) Interface type between CPU and Reader IC&lt;/P&gt;&lt;P&gt;For example, SPI is faster than UART and I2C.&lt;/P&gt;&lt;P&gt;(2) Speed of RF channel&lt;/P&gt;&lt;P&gt;(3) Handling speed of software&lt;/P&gt;&lt;P&gt;(4) Reflection speed of tag&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 07:25:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607401#M827</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-12-14T07:25:31Z</dc:date>
    </item>
    <item>
      <title>Re: Fastest encoder IC</title>
      <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607402#M828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/weidong.sun"&gt;weidong.sun&lt;/A&gt;‌, how you doing?!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yeah, you are right. But the aspects you mentioned&amp;nbsp;are not about the IC only. I think the IC have a lot of operations been done before send the response to a SPI port, for example.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wanna know if a PN532 IC is faster than a RC522, for example, handling all this operations.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 11:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607402#M828</guid>
      <dc:creator>fernandohcoelho</dc:creator>
      <dc:date>2016-12-14T11:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: Fastest encoder IC</title>
      <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607403#M829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Fernando ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I confirmed quesiton on the speed of PN532 &amp;amp; RC522 with NFC technical team, we can't say whose speed is faster, speed is determined by transaction &amp;amp; CPU handling time, not RF firmware( firmware in reader IC ).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Hope above information can help you!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Weidong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 07:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607403#M829</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2016-12-15T07:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: Fastest encoder IC</title>
      <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607404#M830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;speed is not directly determined by the used RF frontend but rather by the overall system partitioning. If you compare both devices, RC522 and PN532 there is one big difference: RC522 is a hard-wired logic, register based frontend. All hardware and protocol abstraction logic has to be implemented on your microcontroller.&amp;nbsp;&lt;/P&gt;&lt;P&gt;PN532, on the other hand, is an integrated NFC controller so hardware and protocol abstraction runs diectly inside PN532 and is tightly coupled with the contactless interface. On host micrcontroller side only a few commands have to be sent in order to activate/detect a tag for instance whilst RC522 requires multiple low level register operations, each operation results in a single SPI/I2C transfer.&amp;nbsp;PN532 performs this low level register operations directly onchip (inside PN532), so one register operations takes not even 1us. Writing a register from a host microcontroller into RC522 can take several hundred microseconds (counting software overhead, SPI/I2C transfer times etc.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So&amp;nbsp;looking at these facts I would say from overall system perspective PN532 could operate much faster than RC522.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Advantage of RC522 of course is a higher flexibility,&amp;nbsp;since host micrcontroller has direct register access to the contatless interface hardware.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;HTH,&lt;/P&gt;&lt;P&gt;Christian.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 07:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607404#M830</guid>
      <dc:creator>christianeisend</dc:creator>
      <dc:date>2016-12-15T07:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: Fastest encoder IC</title>
      <link>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607405#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Christian!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the answer. Now the difference between the two IC become clear.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll buy a PN532 Arduino Shield and run some tests.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again!&lt;/P&gt;&lt;P&gt;Fernando Coelho&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 12:56:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Fastest-encoder-IC/m-p/607405#M831</guid>
      <dc:creator>fernandohcoelho</dc:creator>
      <dc:date>2016-12-15T12:56:32Z</dc:date>
    </item>
  </channel>
</rss>