<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: NHS3100 SPI Questions</title>
    <link>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1248312#M8296</link>
    <description>&lt;P&gt;I move this thread to the correct forum&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Mar 2021 16:28:28 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2021-03-18T16:28:28Z</dc:date>
    <item>
      <title>NHS3100 SPI Questions</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1244186#M8295</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm trying to use SPI and that's why i'm using ssp driver. I'm not an expert in SPI.&lt;/P&gt;&lt;P&gt;I write few simples lines :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;    Chip_SSP_Enable(NSS_SSP0);
    char lenght = Chip_SSP_ReadFrames_Blocking(NSS_SSP0,data,bytesNumber);
    Chip_SSP_Disable(NSS_SSP0);&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;But i was wondering where does i should select to which slave i'm talking ? I couldn't find it.&lt;/P&gt;&lt;P&gt;Thank you for your help and yours answers,&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Yvan&lt;/P&gt;</description>
      <pubDate>Thu, 11 Mar 2021 13:29:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1244186#M8295</guid>
      <dc:creator>SnoZek</dc:creator>
      <dc:date>2021-03-11T13:29:07Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3100 SPI Questions</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1248312#M8296</link>
      <description>&lt;P&gt;I move this thread to the correct forum&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Mar 2021 16:28:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1248312#M8296</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2021-03-18T16:28:28Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3100 SPI Questions</title>
      <link>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1248907#M8303</link>
      <description>&lt;P&gt;Hi Yvan,&lt;/P&gt;
&lt;P&gt;The SPI Chip Select line corresponds to pin SSEL (frame sync select) of the SSP HW block. It is routed to pin 2.&lt;/P&gt;
&lt;P&gt;When the IC drives the clock signal, it will also set it to active state before the start of the serial data. When the IC follows the clock signal, the change to active state qualifies for the presence of data.&lt;BR /&gt;See for more information in the datasheet, &lt;EM&gt;Chapter 8.10,&amp;nbsp;SPI controller&lt;/EM&gt;; basic examples can be found under &lt;EM&gt;&amp;lt;SDK&amp;gt;/docs/firmware.html.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;If you have more than two devices on the SPI bus, you cannot simply connect the chip select pins together, but will need to use multiple pins on the main device, one for each follower that is present. Driving those pins falls outside the scope of the SPI driver.&lt;/P&gt;
&lt;P&gt;KR,&lt;BR /&gt;Dries.&lt;/P&gt;</description>
      <pubDate>Fri, 19 Mar 2021 12:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NHS3100-SPI-Questions/m-p/1248907#M8303</guid>
      <dc:creator>driesmoors</dc:creator>
      <dc:date>2021-03-19T12:21:29Z</dc:date>
    </item>
  </channel>
</rss>