<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: FRDM-K82F interface with RC663</title>
    <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240225#M8253</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/174475"&gt;@sagar_prajapati&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you your reply.&lt;/P&gt;&lt;P&gt;I try the option2 but it can't work in my project.&lt;/P&gt;&lt;P&gt;I use example BasicDiscoveryLoop, it don't have delay can set.&lt;/P&gt;&lt;P&gt;I think maybe my pin define cause some error.&lt;/P&gt;&lt;P&gt;My pin didn't be pulled up in the DAL/board setting.&lt;/P&gt;&lt;P&gt;Thank you your reply again .&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Yen&lt;/P&gt;</description>
    <pubDate>Thu, 04 Mar 2021 11:06:07 GMT</pubDate>
    <dc:creator>yen_chen</dc:creator>
    <dc:date>2021-03-04T11:06:07Z</dc:date>
    <item>
      <title>FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/954912#M6004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have downloaded code from nxp site and made connection as per document. Also define PHDRIVER_FRDM_K82FRC663_BOARD in preprocessor. I am able to read chip id 0x1a but Card is not detected. Please help me to get out of this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sagar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 13:03:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/954912#M6004</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2019-09-05T13:03:48Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/954913#M6005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Code stops at phOsal_sleep() function.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 13:18:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/954913#M6005</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2019-09-05T13:18:46Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/954914#M6006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you download the latest NFC reader library for FRDM-K82F?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81039i30A4DF3B00B7354A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and are you referring to &lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11908.pdf" title="https://www.nxp.com/docs/en/application-note/AN11908.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11908.pdf&lt;/A&gt; ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Were CLEV6630B and FRDM-K82F used on your side?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly clarify.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your patience!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Sep 2019 05:42:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/954914#M6006</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-09-11T05:42:21Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1239995#M8251</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/174475"&gt;@sagar_prajapati&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Are you solved this issue?&lt;/P&gt;&lt;P&gt;If true,could you tell me what to do?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 07:23:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1239995#M8251</guid>
      <dc:creator>yen_chen</dc:creator>
      <dc:date>2021-03-04T07:23:13Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240169#M8252</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180828"&gt;@yen_chen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have solved this issue.&lt;/P&gt;&lt;P&gt;Actually I do not remember exact solution for this but as I remember I have done 2 changes in the code that I suggest you to do.&lt;/P&gt;&lt;P&gt;1. Add minor delay in continous card detection polling loop.&amp;nbsp; I have checked the example for MifareClassic. I am attaching sample code for your reference.&lt;/P&gt;&lt;P&gt;2. Increase heap Size if you are running this code with RTOS. IF you are running with Baremetal then no need to increase heap Size.&amp;nbsp;&lt;/P&gt;&lt;P&gt;do&lt;BR /&gt;{&lt;BR /&gt;/* Field OFF */&lt;BR /&gt;status = phhalHw_FieldOff(pHal);&lt;BR /&gt;CHECK_STATUS(status);&lt;BR /&gt;&lt;BR /&gt;status = phhalHw_Wait(pDiscLoop-&amp;gt;pHalDataParams,PHHAL_HW_TIME_MICROSECONDS, 5100); //5100&lt;BR /&gt;CHECK_STATUS(status);&lt;BR /&gt;&lt;BR /&gt;/* Configure Discovery loop for Poll Mode */&lt;BR /&gt;status = phacDiscLoop_SetConfig(pDiscLoop, PHAC_DISCLOOP_CONFIG_NEXT_POLL_STATE, PHAC_DISCLOOP_POLL_STATE_DETECTION);&lt;BR /&gt;CHECK_STATUS(status);&lt;BR /&gt;&lt;BR /&gt;/* Run Discovery loop */&lt;BR /&gt;status = phacDiscLoop_Run(pDiscLoop, PHAC_DISCLOOP_ENTRY_POINT_POLL);&lt;BR /&gt;vTaskDelay(10);&lt;BR /&gt;&lt;BR /&gt;}while((status &amp;amp; PH_ERR_MASK) != PHAC_DISCLOOP_DEVICE_ACTIVATED); /* Exit on Card detection */&lt;/P&gt;&lt;P&gt;Please do above changes and let me know whether this works or not. If you find any error please let me know I will bring the hardware and test again.&lt;/P&gt;&lt;P&gt;Waiting for your reply.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 09:40:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240169#M8252</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2021-03-04T09:40:06Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240225#M8253</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/174475"&gt;@sagar_prajapati&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you your reply.&lt;/P&gt;&lt;P&gt;I try the option2 but it can't work in my project.&lt;/P&gt;&lt;P&gt;I use example BasicDiscoveryLoop, it don't have delay can set.&lt;/P&gt;&lt;P&gt;I think maybe my pin define cause some error.&lt;/P&gt;&lt;P&gt;My pin didn't be pulled up in the DAL/board setting.&lt;/P&gt;&lt;P&gt;Thank you your reply again .&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Yen&lt;/P&gt;</description>
      <pubDate>Thu, 04 Mar 2021 11:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240225#M8253</guid>
      <dc:creator>yen_chen</dc:creator>
      <dc:date>2021-03-04T11:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240737#M8254</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/180828"&gt;@yen_chen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Give me some time I will collect hardware and check and update you.&amp;nbsp; I will also run basicdiscovery loop example.&lt;/P&gt;</description>
      <pubDate>Fri, 05 Mar 2021 06:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1240737#M8254</guid>
      <dc:creator>sagar_prajapati</dc:creator>
      <dc:date>2021-03-05T06:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K82F interface with RC663</title>
      <link>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1270946#M8488</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am also faciing same problem. Code stucks in phOsal_sleep function that is called from&amp;nbsp;phOsal_EventPend fuunction. can you please look into this and update as soon as possible?&lt;/P&gt;</description>
      <pubDate>Fri, 30 Apr 2021 16:14:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/FRDM-K82F-interface-with-RC663/m-p/1270946#M8488</guid>
      <dc:creator>sagarprajapati</dc:creator>
      <dc:date>2021-04-30T16:14:47Z</dc:date>
    </item>
  </channel>
</rss>