<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DPC at Power-On at PN7462 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/DPC-at-Power-On-at-PN7462/m-p/1237244#M8238</link>
    <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I found the error myself: long story short: Soldering mistake!&lt;/P&gt;</description>
    <pubDate>Fri, 26 Feb 2021 10:42:58 GMT</pubDate>
    <dc:creator>johannesdev</dc:creator>
    <dc:date>2021-02-26T10:42:58Z</dc:date>
    <item>
      <title>DPC at Power-On at PN7462</title>
      <link>https://community.nxp.com/t5/NFC/DPC-at-Power-On-at-PN7462/m-p/1236667#M8233</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I'm designing an application with the PN7462 and its DPC. Currently I have 3 gears implemented with the NFC cockpit. Using an oscilloscope and an EMVCo TestPICC I can see the gears switching up and down when changing the distance between the NFC antenna and the TestPICC. So far, so good.&lt;/P&gt;&lt;P&gt;However, when I switch on the field using the cockpit, I see the following waveform (on DC-Out of the TestPICC which is at z=0cm):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="johannesdev_0-1614262410568.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/138123i75CFC91B3D700B41/image-size/medium?v=v2&amp;amp;px=400" role="button" title="johannesdev_0-1614262410568.png" alt="johannesdev_0-1614262410568.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It seems that the DPC starts at the lowest gear with the highest voltage, &lt;STRONG&gt;possibly harming the PN7462's output stage&lt;/STRONG&gt;. Certainly, this is because I set the DPC-Control Byte (at 0x201352) to 0x13 (=Start Gear 1, DPC enabled, Gear Step 1).&lt;/P&gt;&lt;P&gt;When reading AN11742 it seems to me, that the DPC Control byte has to be 0x33 as I have 3 gears active. However, in this case the DPC does not work at all. Here the DPC stays at gear 0 all the time, regardless of how high the AGC-Value rises.&lt;/P&gt;&lt;P&gt;So how to start the DPC at gear 3 at power on? What do I get wrong?&lt;/P&gt;&lt;P&gt;Thank you for any help!&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 14:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/DPC-at-Power-On-at-PN7462/m-p/1236667#M8233</guid>
      <dc:creator>johannesdev</dc:creator>
      <dc:date>2021-02-25T14:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: DPC at Power-On at PN7462</title>
      <link>https://community.nxp.com/t5/NFC/DPC-at-Power-On-at-PN7462/m-p/1237244#M8238</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;I found the error myself: long story short: Soldering mistake!&lt;/P&gt;</description>
      <pubDate>Fri, 26 Feb 2021 10:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/DPC-at-Power-On-at-PN7462/m-p/1237244#M8238</guid>
      <dc:creator>johannesdev</dc:creator>
      <dc:date>2021-02-26T10:42:58Z</dc:date>
    </item>
  </channel>
</rss>