<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic My CLRC663 reader keeps giving interrupt in LPCD mode in NFC</title>
    <link>https://community.nxp.com/t5/NFC/My-CLRC663-reader-keeps-giving-interrupt-in-LPCD-mode/m-p/1229284#M8182</link>
    <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on RFID project and am using CLRC663 plus reader and STM32L0. So far I could read UID, atqa, and managed to read and write from/to tag. Now I am working on LPCD mode and am tuning my antenna to get the best range however the problem is my project needs very low power consumption at the moment I am getting 1.5mA in LPCD mode which is far more than I am expecting and I think the reason is my continuous interrupt, i am getting in IRQ pin! which is a bit strange! all my interrupts are disabled and only LPCD interrupt is enabled and I do not understand why I keep getting interrupt even when the card is not presented! Going deep into this, I found out that this interrupt is happening exactly at the time T4 is underflows however T4 is not set to give interrupt! I am so confused. Does anyone have the same problem or Is it at all normal to get interrupt in LPCD mode continuously? I really appreciate any help.Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 10 Feb 2021 12:13:32 GMT</pubDate>
    <dc:creator>minabf61</dc:creator>
    <dc:date>2021-02-10T12:13:32Z</dc:date>
    <item>
      <title>My CLRC663 reader keeps giving interrupt in LPCD mode</title>
      <link>https://community.nxp.com/t5/NFC/My-CLRC663-reader-keeps-giving-interrupt-in-LPCD-mode/m-p/1229284#M8182</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am working on RFID project and am using CLRC663 plus reader and STM32L0. So far I could read UID, atqa, and managed to read and write from/to tag. Now I am working on LPCD mode and am tuning my antenna to get the best range however the problem is my project needs very low power consumption at the moment I am getting 1.5mA in LPCD mode which is far more than I am expecting and I think the reason is my continuous interrupt, i am getting in IRQ pin! which is a bit strange! all my interrupts are disabled and only LPCD interrupt is enabled and I do not understand why I keep getting interrupt even when the card is not presented! Going deep into this, I found out that this interrupt is happening exactly at the time T4 is underflows however T4 is not set to give interrupt! I am so confused. Does anyone have the same problem or Is it at all normal to get interrupt in LPCD mode continuously? I really appreciate any help.Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 10 Feb 2021 12:13:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/My-CLRC663-reader-keeps-giving-interrupt-in-LPCD-mode/m-p/1229284#M8182</guid>
      <dc:creator>minabf61</dc:creator>
      <dc:date>2021-02-10T12:13:32Z</dc:date>
    </item>
  </channel>
</rss>