<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックMF1ICS50 add external power supply</title>
    <link>https://community.nxp.com/t5/NFC/MF1ICS50-add-external-power-supply/m-p/1227597#M8166</link>
    <description>&lt;P&gt;Hello.&amp;nbsp;MF1ICS50 chip is a passive NFC tag that is supposed to be connected to an antenna in parallel and draw power from the reader device EM field. I want to add an external power supply to it, effectively making it an "active" tag, thus boosting read range. Is it possible? Can somebody give me a circuit diagram or at least some hints? Perhaps using LM358 amplifier.&lt;/P&gt;</description>
    <pubDate>Sun, 07 Feb 2021 21:49:38 GMT</pubDate>
    <dc:creator>plentypvp</dc:creator>
    <dc:date>2021-02-07T21:49:38Z</dc:date>
    <item>
      <title>MF1ICS50 add external power supply</title>
      <link>https://community.nxp.com/t5/NFC/MF1ICS50-add-external-power-supply/m-p/1227597#M8166</link>
      <description>&lt;P&gt;Hello.&amp;nbsp;MF1ICS50 chip is a passive NFC tag that is supposed to be connected to an antenna in parallel and draw power from the reader device EM field. I want to add an external power supply to it, effectively making it an "active" tag, thus boosting read range. Is it possible? Can somebody give me a circuit diagram or at least some hints? Perhaps using LM358 amplifier.&lt;/P&gt;</description>
      <pubDate>Sun, 07 Feb 2021 21:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MF1ICS50-add-external-power-supply/m-p/1227597#M8166</guid>
      <dc:creator>plentypvp</dc:creator>
      <dc:date>2021-02-07T21:49:38Z</dc:date>
    </item>
  </channel>
</rss>