<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ICODE DNA freeze (No reply) until RF Off in NFC</title>
    <link>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1226038#M8146</link>
    <description>&lt;P&gt;Hello Patrick and Jonathan,&lt;/P&gt;&lt;P&gt;We are experiencing a similar problem and seeing around a 1.5% fallout. Were you seeing a similar fallout/defect rate?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Were you able to root cause this to the tag manufacturer, material, or antenna tuning issue? Did you find a resolution?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;John&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 04 Feb 2021 03:30:31 GMT</pubDate>
    <dc:creator>John_G</dc:creator>
    <dc:date>2021-02-04T03:30:31Z</dc:date>
    <item>
      <title>ICODE DNA freeze (No reply) until RF Off</title>
      <link>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002473#M6558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;We use the ICODE DNA chip on inlays with our own RFID reader.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;On some tags, sometime the chip doesn't reply on an addressed read single block command and after that, the chip seems to be frozen. We have to switch off / switch on the RF signal to return to nominal operation.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;The freeze can also occur on a mutual authentication command.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;This happens with several readers, several different environments and only on some chips.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92358i94083E910528096B/image-size/large?v=v2&amp;amp;px=999" title="Issue.png" alt="Issue.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Is someone experiments the same kind of issue with ICODE DNA?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;What can be the root cause of a total freeze of the chip ?&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;Patrick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2019 16:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002473#M6558</guid>
      <dc:creator>psoto</dc:creator>
      <dc:date>2019-11-04T16:48:11Z</dc:date>
    </item>
    <item>
      <title>Re: ICODE DNA freeze (No reply) until RF Off</title>
      <link>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002474#M6559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="323116" data-username="psoto" href="https://community.nxp.com/people/psoto"&gt;Patrick Soto&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great as you may know the information regarding ICODE DNA is secured under NDA ( Non Disclosure Agreement ) this means that all the information, tools and support should be delivered using secured communication channels and only with customers with active NDA.&amp;nbsp; so we cannot discuss much of the features under NDA in this forum,&amp;nbsp; but&amp;nbsp; do you happen to have an NXP reader ? is it possible for you to use our examples in the library to interact with the ICODE DNA ?&amp;nbsp; to see&amp;nbsp; if the tag is having the problem or if it is the communication with your reader.&lt;/P&gt;&lt;P&gt;Have a great day !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Nov 2019 01:27:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002474#M6559</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2019-11-12T01:27:17Z</dc:date>
    </item>
    <item>
      <title>Re: ICODE DNA freeze (No reply) until RF Off</title>
      <link>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002475#M6560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;We are under NDA with NXP and we have all the documentation needed.&lt;/P&gt;&lt;P&gt;We don't use an NXP reader but this issue is seen on several different readers, based on different firmware and front-end. And the issue occurs on ISO15693 standard commands, so to me, any reader should work with this chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the first write on this thread, I discovered that if I push on the chip stuck on the inlay, the issue disappears. It seems linked to the sticking of the chip&lt;/P&gt;&lt;P&gt;However, to understanding well, what can be the root cause of the freeze of the chip in this case: Is it a serial impedance between chip and antenna which decrease the efficiency of the power supply and the voltage is close to the lower limit ?&lt;/P&gt;&lt;P&gt;Do you see another explanation ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 07:10:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002475#M6560</guid>
      <dc:creator>psoto</dc:creator>
      <dc:date>2019-11-22T07:10:16Z</dc:date>
    </item>
    <item>
      <title>Re: ICODE DNA freeze (No reply) until RF Off</title>
      <link>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002476#M6561</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Patrick I would confirm with the manufacturer of the tag, to see if the&amp;nbsp; materials being used in the tag might be&amp;nbsp; affecting the behavior of the tag, have you tried with other manufacturer tags ? or with other form factors ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;'BR&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2019 01:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1002476#M6561</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2019-11-28T01:33:05Z</dc:date>
    </item>
    <item>
      <title>Re: ICODE DNA freeze (No reply) until RF Off</title>
      <link>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1226038#M8146</link>
      <description>&lt;P&gt;Hello Patrick and Jonathan,&lt;/P&gt;&lt;P&gt;We are experiencing a similar problem and seeing around a 1.5% fallout. Were you seeing a similar fallout/defect rate?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Were you able to root cause this to the tag manufacturer, material, or antenna tuning issue? Did you find a resolution?&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;John&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Feb 2021 03:30:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/ICODE-DNA-freeze-No-reply-until-RF-Off/m-p/1226038#M8146</guid>
      <dc:creator>John_G</dc:creator>
      <dc:date>2021-02-04T03:30:31Z</dc:date>
    </item>
  </channel>
</rss>