<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Maximum range with CLRC663  plus up-to 1m</title>
    <link>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208700#M8054</link>
    <description>&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;I've reviewed those thread earlier but which do not get a clear picture about the range with the SLIX 2 tag.&lt;/P&gt;&lt;P&gt;So asking again Is the EVK tested with SLIX2 Tag? If so what's the max range possible?&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jan 2021 04:55:36 GMT</pubDate>
    <dc:creator>lakshminarayana</dc:creator>
    <dc:date>2021-01-08T04:55:36Z</dc:date>
    <item>
      <title>Maximum range with CLRC663  plus up-to 1m</title>
      <link>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208177#M8047</link>
      <description>&lt;P&gt;May I know what maximum range can be achieved with&amp;nbsp;CLRC663 plus?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I read that it can up to 1.5meters but in the forum, it's mentioned as around 30cm.&lt;/P&gt;&lt;P&gt;With CLRC663 plus, ICODE SLIX 2 Tag can we achieve a range of 1m?&lt;/P&gt;&lt;P&gt;Is the development board&amp;nbsp;CLRC663 plus tested with ICODE SLIX2? If yes what's the maximum range.&lt;/P&gt;&lt;P&gt;Could you please guide us to some of the manufacturers of ICODE SLIX2 tags?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jan 2021 09:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208177#M8047</guid>
      <dc:creator>lakshminarayana</dc:creator>
      <dc:date>2021-01-07T09:50:47Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum range with CLRC663  plus up-to 1m</title>
      <link>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208645#M8051</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;For more information please refer to the&amp;nbsp; thread&amp;nbsp;&lt;A href="https://community.nxp.com/t5/Other-NXP-Products/CLRC663-Long-range-reader-up-to-50cm/td-p/1204941" target="_blank"&gt;https://community.nxp.com/t5/Other-NXP-Products/CLRC663-Long-range-reader-up-to-50cm/td-p/1204941&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;And you can test the board performance of CLRC663 Plus as the link.&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/clrc663-iplus-i-nfc-frontend-development-kit-for-access-management-applications:OM26630FDK" target="_blank"&gt;https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/clrc663-iplus-i-nfc-frontend-development-kit-for-access-management-applications:OM26630FDK&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Hope it help you. Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 02:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208645#M8051</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2021-01-08T02:54:07Z</dc:date>
    </item>
    <item>
      <title>Re: Maximum range with CLRC663  plus up-to 1m</title>
      <link>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208700#M8054</link>
      <description>&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;I've reviewed those thread earlier but which do not get a clear picture about the range with the SLIX 2 tag.&lt;/P&gt;&lt;P&gt;So asking again Is the EVK tested with SLIX2 Tag? If so what's the max range possible?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jan 2021 04:55:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Maximum-range-with-CLRC663-plus-up-to-1m/m-p/1208700#M8054</guid>
      <dc:creator>lakshminarayana</dc:creator>
      <dc:date>2021-01-08T04:55:36Z</dc:date>
    </item>
  </channel>
</rss>