<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックLow frequency long range RFID reader</title>
    <link>https://community.nxp.com/t5/NFC/Low-frequency-long-range-RFID-reader/m-p/605678#M804</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to do a project involving low frequency RFIDs (125-134.2 kHz) and the HTRM902 long range reader kit seems to be obsolete. Is there any other device/IC capable of doing long range RFID tag reading?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Low frequency RFIDs are essential to the project because all of the communication must happen under salty water and high frequencies don't work very well under these conditions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Besides, I'm also wondering if the HTRC11001T IC is able to do long range (0.5 m or more in an air environment) reading with a proper antenna.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Koldo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Oct 2016 12:37:42 GMT</pubDate>
    <dc:creator>koldo52</dc:creator>
    <dc:date>2016-10-26T12:37:42Z</dc:date>
    <item>
      <title>Low frequency long range RFID reader</title>
      <link>https://community.nxp.com/t5/NFC/Low-frequency-long-range-RFID-reader/m-p/605678#M804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to do a project involving low frequency RFIDs (125-134.2 kHz) and the HTRM902 long range reader kit seems to be obsolete. Is there any other device/IC capable of doing long range RFID tag reading?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Low frequency RFIDs are essential to the project because all of the communication must happen under salty water and high frequencies don't work very well under these conditions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Besides, I'm also wondering if the HTRC11001T IC is able to do long range (0.5 m or more in an air environment) reading with a proper antenna.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Koldo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Oct 2016 12:37:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Low-frequency-long-range-RFID-reader/m-p/605678#M804</guid>
      <dc:creator>koldo52</dc:creator>
      <dc:date>2016-10-26T12:37:42Z</dc:date>
    </item>
  </channel>
</rss>