<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Automate PN7462 programming in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1198871#M7959</link>
    <description>&lt;P&gt;Hello, guys.&lt;/P&gt;&lt;P&gt;We have a plan to implement PN7462 RFID reader SoC into our future device. We are considering the possibilities of remote/automated code update of PN7462 module.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we have PN7462 connected with Raspberry Pi over USB, can we use RESET and DWL_REQ pins of PN7462 to set it into download mode so that we can send new flash files from RPi by using some .sh script, for example?&lt;/P&gt;&lt;P&gt;Thanks in advance for your time and efforts.&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Bojan.&lt;/P&gt;</description>
    <pubDate>Mon, 14 Dec 2020 12:26:14 GMT</pubDate>
    <dc:creator>bojankoce</dc:creator>
    <dc:date>2020-12-14T12:26:14Z</dc:date>
    <item>
      <title>Automate PN7462 programming</title>
      <link>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1198871#M7959</link>
      <description>&lt;P&gt;Hello, guys.&lt;/P&gt;&lt;P&gt;We have a plan to implement PN7462 RFID reader SoC into our future device. We are considering the possibilities of remote/automated code update of PN7462 module.&amp;nbsp;&lt;/P&gt;&lt;P&gt;If we have PN7462 connected with Raspberry Pi over USB, can we use RESET and DWL_REQ pins of PN7462 to set it into download mode so that we can send new flash files from RPi by using some .sh script, for example?&lt;/P&gt;&lt;P&gt;Thanks in advance for your time and efforts.&lt;/P&gt;&lt;P&gt;Sincerely,&lt;/P&gt;&lt;P&gt;Bojan.&lt;/P&gt;</description>
      <pubDate>Mon, 14 Dec 2020 12:26:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1198871#M7959</guid>
      <dc:creator>bojankoce</dc:creator>
      <dc:date>2020-12-14T12:26:14Z</dc:date>
    </item>
    <item>
      <title>Re: Automate PN7462 programming</title>
      <link>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1201114#M7972</link>
      <description>&lt;P&gt;Any feedback on this?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Dec 2020 09:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1201114#M7972</guid>
      <dc:creator>bojankoce</dc:creator>
      <dc:date>2020-12-17T09:04:27Z</dc:date>
    </item>
    <item>
      <title>Re: Automate PN7462 programming</title>
      <link>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1204090#M7992</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/181403"&gt;@bojankoce&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes, it is possible. Please kindly refer to 8.10 in&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/UM10883.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/UM10883.pdf&lt;/A&gt;&amp;nbsp;for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 24 Dec 2020 09:55:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Automate-PN7462-programming/m-p/1204090#M7992</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-12-24T09:55:35Z</dc:date>
    </item>
  </channel>
</rss>