<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 CLRC663 and I2C</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1173209#M7839</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi, everyone!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am developing Nfc reader for&amp;nbsp;home access systems.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've the STM32F207 and&amp;nbsp;CLRC663. They communicate&amp;nbsp;via I2C interface.&lt;/P&gt;&lt;P&gt;Bus frequency is 400 kHz.&amp;nbsp;In the system has&amp;nbsp;another I2C device on same bus.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Сan there be problems in the operation of the CLRC663 if there is another parallel operating device?&lt;/P&gt;&lt;P&gt;Or is it better to leave only CLRC663 on the bus?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 26 Oct 2020 14:58:30 GMT</pubDate>
    <dc:creator>fomin-ruslan32</dc:creator>
    <dc:date>2020-10-26T14:58:30Z</dc:date>
    <item>
      <title>CLRC663 and I2C</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1173209#M7839</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, everyone!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I am developing Nfc reader for&amp;nbsp;home access systems.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've the STM32F207 and&amp;nbsp;CLRC663. They communicate&amp;nbsp;via I2C interface.&lt;/P&gt;&lt;P&gt;Bus frequency is 400 kHz.&amp;nbsp;In the system has&amp;nbsp;another I2C device on same bus.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Сan there be problems in the operation of the CLRC663 if there is another parallel operating device?&lt;/P&gt;&lt;P&gt;Or is it better to leave only CLRC663 on the bus?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 14:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1173209#M7839</guid>
      <dc:creator>fomin-ruslan32</dc:creator>
      <dc:date>2020-10-26T14:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 and I2C</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1174026#M7844</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. There should be no problem having two devices on an I2C bus, but it would be better to have just one I2C bus for the CLRC663.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 18:12:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1174026#M7844</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-10-27T18:12:19Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 and I2C</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1181160#M7875</link>
      <description>&lt;P&gt;Are there any examples or existing code that shows a working state using i2c? All the existing examples seem to be biased toward SPI.&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 02:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1181160#M7875</guid>
      <dc:creator>Gaolaowai</dc:creator>
      <dc:date>2020-11-11T02:52:19Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 and I2C</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1188742#M7918</link>
      <description>&lt;P&gt;If you can read and write clrc663 registers through i2c then the i2c interface is working.&amp;nbsp;But there is a nuance, if the bus frequency is higher than 100 kHz, you must wait a while until the command is processed.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 08:17:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1188742#M7918</guid>
      <dc:creator>fomin-ruslan32</dc:creator>
      <dc:date>2020-11-25T08:17:54Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 and I2C</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1188744#M7919</link>
      <description>&lt;P&gt;hi, Ricardo!&lt;/P&gt;&lt;P&gt;Thanks a lot of answer.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 08:20:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-and-I2C/m-p/1188744#M7919</guid>
      <dc:creator>fomin-ruslan32</dc:creator>
      <dc:date>2020-11-25T08:20:16Z</dc:date>
    </item>
  </channel>
</rss>