<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Help. Can´t get Anticollsion loop with two PICCs.</title>
    <link>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1167007#M7802</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please help me with more information of the MCU you are using as a host ? firmware you are using, if you can provide a link it would be helpful.&amp;nbsp; ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards, &lt;BR /&gt;Estephania&lt;/P&gt;</description>
    <pubDate>Wed, 14 Oct 2020 00:54:18 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2020-10-14T00:54:18Z</dc:date>
    <item>
      <title>Help. Can´t get Anticollsion loop with two PICCs.</title>
      <link>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1163324#M7773</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I´m working with RC522 and I´m dealing with the anticolision loop when two tags are shown in the antenna. The two tags I am working with have the following UIDs:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PICC #1:&amp;nbsp; 86 A0 83 EE&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PICC #2:&amp;nbsp; 16 9A 0A 3B&lt;/P&gt;&lt;P&gt;When PCD sends SEL + NVB (0x93 + 0x20), both PICC answer and the information I get from the registers is the following:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ComIrqReg&lt;/STRONG&gt;: 0x66.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Bit TxIRq = 1.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Bit RxIRq = 1.&amp;nbsp; (The end of a valid stream detected)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/STRONG&gt;Bit ErrIRq = 1. (Error bit in ErrorReg is set)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ErrorReg&lt;/STRONG&gt;: 0x08.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Bit CollErr = 1. (A collision detected)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;CollErr&lt;/STRONG&gt;: 0x05.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Bit CollPosNotValid = 0&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;Bit CollPos[4..0] = 05.&amp;nbsp; (Collision in the fifth bit.)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Let´s confirm the collision is in the fifth bit:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;PICC #1 UID0 = 0x86 = 100&lt;FONT color="#FF0000"&gt;0&lt;/FONT&gt; 0110&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;PICC #2 UID0 = 0x16 = 000&lt;FONT color="#FF0000"&gt;1&lt;/FONT&gt; 0110&lt;/P&gt;&lt;P&gt;However my doubts are about the information PCD has to send back to the PICC and the value of BitFrammingReg Register:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; BitFrammingReg=0x55&amp;nbsp; &amp;nbsp; and&amp;nbsp; &amp;nbsp; &amp;nbsp; SEL (0x93) + NVD (0x25)+ &lt;FONT color="#FF0000"&gt;1&lt;/FONT&gt;0110 ?????&lt;/P&gt;&lt;P&gt;Or&amp;nbsp; &amp;nbsp; &amp;nbsp; BitFrammingReg=0x55&amp;nbsp; &amp;nbsp; and&amp;nbsp; &amp;nbsp; &amp;nbsp; SEL (0x93) + NVD (0x25)+ 0110&lt;FONT color="#FF0000"&gt;1&lt;/FONT&gt; ?????&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I tried different options but I'm not able to succeed. Please find attached the code file in case somebody could have a look and give me a clue.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help will be apreciated. Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Oct 2020 09:30:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1163324#M7773</guid>
      <dc:creator>patricio</dc:creator>
      <dc:date>2020-10-06T09:30:27Z</dc:date>
    </item>
    <item>
      <title>Re: Help. Can´t get Anticollsion loop with two PICCs.</title>
      <link>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1167007#M7802</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please help me with more information of the MCU you are using as a host ? firmware you are using, if you can provide a link it would be helpful.&amp;nbsp; ?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards, &lt;BR /&gt;Estephania&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 00:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1167007#M7802</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2020-10-14T00:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: Help. Can´t get Anticollsion loop with two PICCs.</title>
      <link>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1170724#M7829</link>
      <description>&lt;P&gt;Hello Estephania,&lt;/P&gt;&lt;P&gt;Thank you for your reply. It is solved already.&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR.&lt;/P&gt;</description>
      <pubDate>Wed, 21 Oct 2020 06:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Help-Can-t-get-Anticollsion-loop-with-two-PICCs/m-p/1170724#M7829</guid>
      <dc:creator>patricio</dc:creator>
      <dc:date>2020-10-21T06:00:17Z</dc:date>
    </item>
  </channel>
</rss>