<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NTAG based Systems - Regulatory Testing Requirements - FCC / CE in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-based-Systems-Regulatory-Testing-Requirements-FCC-CE/m-p/604768#M777</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a system involved MCU and oscillation circuit then FCC is required.&lt;BR /&gt;For our OM5569 demo set, it included two part, one is NTAG I2C plus board, and the other is LCD displayer which embedded with LCD display, MCU and sensor that required FCC certification.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope that makes sense,&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Dec 2016 07:20:48 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2016-12-29T07:20:48Z</dc:date>
    <item>
      <title>NTAG based Systems - Regulatory Testing Requirements - FCC / CE</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-based-Systems-Regulatory-Testing-Requirements-FCC-CE/m-p/604767#M776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;Normally an RFID / NFC tag is a considered a passive device and FCC testing is not required. &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;However, &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;When you add a microcontroller and other peripherals that start clocking at different frequencies than the 13.56 carrier frequency, experience says that you get an unintentional radiator. &amp;nbsp; &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;1. So the question is do systems as described above require FCC and/or CE Testing?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;2. If not, please explain why these are not considered unintentional radiators?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; color: #1f497d;"&gt;3. Also - why does the the NTAG Demo board contain an FCC-ID: OWROM5569-NT322E.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 22:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-based-Systems-Regulatory-Testing-Requirements-FCC-CE/m-p/604767#M776</guid>
      <dc:creator>davidsherrets</dc:creator>
      <dc:date>2016-12-12T22:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG based Systems - Regulatory Testing Requirements - FCC / CE</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-based-Systems-Regulatory-Testing-Requirements-FCC-CE/m-p/604768#M777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If a system involved MCU and oscillation circuit then FCC is required.&lt;BR /&gt;For our OM5569 demo set, it included two part, one is NTAG I2C plus board, and the other is LCD displayer which embedded with LCD display, MCU and sensor that required FCC certification.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope that makes sense,&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Dec 2016 07:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-based-Systems-Regulatory-Testing-Requirements-FCC-CE/m-p/604768#M777</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2016-12-29T07:20:48Z</dc:date>
    </item>
  </channel>
</rss>