<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ntag 424DNA write lock failed while using android Native method in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1158878#M7734</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I dont think the same process as an NTAG216 can apply to an NTAG 424,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the NTAG is a T2T which means that the capability container and the protection is handled&amp;nbsp; by a PROT register and a PWD.&amp;nbsp; for NTGA 424 is different since it is a T4T the capability container is not in a memory sector like NTAG 215 is in a file inside the NTAG 424&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jonathaniglesia_0-1600979829336.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126137i4FC33F4D1CA61D69/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jonathaniglesia_0-1600979829336.png" alt="jonathaniglesia_0-1600979829336.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;in order to interact with this you should first select the FID, then authenticate to the NTAG 424 then modify the value of the CC file.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please check if there is some API for T4T or please perform the sequence to modify the NTAG 424 CC file and also&amp;nbsp; it would be good that you change the write, change and R/W access key to a known key or if you dont want anybody to using this in the future change them to F,&amp;nbsp; and just leave the read value to E to everyone can read the NDEF file.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;maybe you can use as reference the following post&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NFC/Change-Keys-and-quot-lock-quot-NTAG-DNA-424/m-p/1058607#M7158" target="_blank"&gt;https://community.nxp.com/t5/NFC/Change-Keys-and-quot-lock-quot-NTAG-DNA-424/m-p/1058607#M7158&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;it does not uses a code example or something but you can see how is the process and apply it to your code.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&lt;/P&gt;</description>
    <pubDate>Thu, 24 Sep 2020 20:42:02 GMT</pubDate>
    <dc:creator>Jonathan_Iglesias</dc:creator>
    <dc:date>2020-09-24T20:42:02Z</dc:date>
    <item>
      <title>Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1157635#M7731</link>
      <description>&lt;P&gt;We have a React native mobile application which write some data (NDEF) to NTAG 424 DNA. After writing Tag needs to be write locked.&lt;/P&gt;&lt;P&gt;For write locking purpose, used android default method makeReadonly(). But it failing on tag 424 DNA.&lt;/P&gt;&lt;P&gt;I was able to format and Write-lock with NXP tagWriter android application. but not with android API s&lt;/P&gt;&lt;P&gt;Given below is tag info which I used:-&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class="pun"&gt;{&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"canMakeReadOnly"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:&lt;/SPAN&gt;&lt;SPAN class="kwd"&gt;false&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"id"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:&lt;/SPAN&gt;&lt;SPAN class="str"&gt;"043743CE80"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"isWritable"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:&lt;/SPAN&gt;&lt;SPAN class="kwd"&gt;true&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"maxSize"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:&lt;/SPAN&gt;&lt;SPAN class="lit"&gt;254&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"ndefMessage"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:[],&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"techTypes"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:[&lt;/SPAN&gt;
      &lt;SPAN class="str"&gt;"android.nfc.tech.IsoDep"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;
      &lt;SPAN class="str"&gt;"android.nfc.tech.NfcA"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;
      &lt;SPAN class="str"&gt;"android.nfc.tech.Ndef"&lt;/SPAN&gt;
   &lt;SPAN class="pun"&gt;],&lt;/SPAN&gt;
   &lt;SPAN class="str"&gt;"type"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;:&lt;/SPAN&gt;&lt;SPAN class="str"&gt;"NFC Forum Type 4"&lt;/SPAN&gt;
&lt;SPAN class="pun"&gt;}&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;Here is a part of code which Currently using&lt;/P&gt;&lt;PRE&gt;&lt;SPAN class="kwd"&gt;try&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;{&lt;/SPAN&gt;
&lt;SPAN class="kwd"&gt;await&lt;/SPAN&gt; &lt;SPAN class="typ"&gt;NfcManager&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;.&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;writeNdefMessage&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;(&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;bytes&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;)&lt;/SPAN&gt;
        &lt;SPAN class="pun"&gt;.&lt;/SPAN&gt;&lt;SPAN class="kwd"&gt;then&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;(()=&amp;gt;&lt;/SPAN&gt;&lt;SPAN class="typ"&gt;NfcManager&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;.&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;makeReadOnlyAndroid&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;())&lt;/SPAN&gt;
        &lt;SPAN class="pun"&gt;.&lt;/SPAN&gt;&lt;SPAN class="kwd"&gt;then&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;((&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;result&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;)=&amp;gt;{&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;          console&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;.&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;log&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;(&lt;/SPAN&gt;&lt;SPAN class="str"&gt;"Make read Only result:-&amp;gt;"&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;result&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;);&lt;/SPAN&gt;
        &lt;SPAN class="pun"&gt;});&lt;/SPAN&gt;
&lt;SPAN class="pun"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="kwd"&gt;catch&lt;/SPAN&gt; &lt;SPAN class="pun"&gt;(&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;ex&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;)&lt;/SPAN&gt; &lt;SPAN class="pun"&gt;{&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;      console&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;.&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;warn&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;(&lt;/SPAN&gt;&lt;SPAN class="str"&gt;'exception'&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;,&lt;/SPAN&gt;&lt;SPAN class="pln"&gt; ex&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;);&lt;/SPAN&gt;&lt;SPAN class="pln"&gt;      _cleanUp&lt;/SPAN&gt;&lt;SPAN class="pun"&gt;();&lt;/SPAN&gt;
     
    &lt;SPAN class="pun"&gt;}&lt;/SPAN&gt;&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;The same is working for "NTAG216"&amp;nbsp;&lt;/P&gt;&lt;P&gt;{"canMakeReadOnly": true, "id": "04883C82B25680", "isWritable": true, "maxSize": 868, "ndefMessage": [{"id": "", "payload": [Array], "tnf": 1, "type": [Array]}], "techTypes": ["android.nfc.tech.NfcA", "android.nfc.tech.MifareUltralight", "android.nfc.tech.Ndef"], "type": "NFC Forum Type 2"}&lt;/P&gt;&lt;P&gt;for react native i have also used&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;A href="https://github.com/whitedogg13/react-native-nfc-manager" target="_blank" rel="noopener"&gt;https://github.com/whitedogg13/react-native-nfc-manager&lt;/A&gt;&lt;/STRONG&gt; :- this plugin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 09:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1157635#M7731</guid>
      <dc:creator>Anandhu</dc:creator>
      <dc:date>2020-09-23T09:07:02Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1158878#M7734</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I dont think the same process as an NTAG216 can apply to an NTAG 424,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the NTAG is a T2T which means that the capability container and the protection is handled&amp;nbsp; by a PROT register and a PWD.&amp;nbsp; for NTGA 424 is different since it is a T4T the capability container is not in a memory sector like NTAG 215 is in a file inside the NTAG 424&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jonathaniglesia_0-1600979829336.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126137i4FC33F4D1CA61D69/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jonathaniglesia_0-1600979829336.png" alt="jonathaniglesia_0-1600979829336.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;in order to interact with this you should first select the FID, then authenticate to the NTAG 424 then modify the value of the CC file.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please check if there is some API for T4T or please perform the sequence to modify the NTAG 424 CC file and also&amp;nbsp; it would be good that you change the write, change and R/W access key to a known key or if you dont want anybody to using this in the future change them to F,&amp;nbsp; and just leave the read value to E to everyone can read the NDEF file.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;maybe you can use as reference the following post&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/NFC/Change-Keys-and-quot-lock-quot-NTAG-DNA-424/m-p/1058607#M7158" target="_blank"&gt;https://community.nxp.com/t5/NFC/Change-Keys-and-quot-lock-quot-NTAG-DNA-424/m-p/1058607#M7158&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;it does not uses a code example or something but you can see how is the process and apply it to your code.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&lt;/P&gt;</description>
      <pubDate>Thu, 24 Sep 2020 20:42:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1158878#M7734</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-09-24T20:42:02Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1159300#M7738</link>
      <description>&lt;P&gt;Hope their is only&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;[NfcTech].transceive([0x00,etc..])&lt;/PRE&gt;&lt;P&gt;but am completely confused with these hexadecimal part. Is it possible to read and modify CC file using these commands,&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 11:02:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1159300#M7738</guid>
      <dc:creator>Anandhu</dc:creator>
      <dc:date>2020-09-25T11:02:39Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1159403#M7740</link>
      <description>&lt;P&gt;I am sorry but I dont completely understand this reply, can you please elaborate more on this.&lt;/P&gt;&lt;P&gt;also please confirm you are using the DS of NTAG 424?&amp;nbsp; because all of this is explained there, also in the features and hints you can find examples of how to do some things on NTAG 424.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/NT4H2421Gx.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/NT4H2421Gx.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;in section 5.1 you can see the user memory and the explanation of the CC file also section 10 for the command set like write and read.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12196.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12196.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;in section 6 there is a personalization example where you can see how to modify the CC file.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 14:36:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1159403#M7740</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-09-25T14:36:59Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1159734#M7743</link>
      <description>&lt;P&gt;Hi Jonathan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks for your support. I've just consolidated the steps I did into a file. This may give you a clear understanding of where I'm stuck.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://docs.google.com/document/d/16lOoh2Fuo6cTDzgddQXz4VOy0K8mGEaIIApeJdeNMhw/edit?usp=sharing" target="_blank"&gt;https://docs.google.com/document/d/16lOoh2Fuo6cTDzgddQXz4VOy0K8mGEaIIApeJdeNMhw/edit?usp=sharing&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Anandhu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Sep 2020 12:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1159734#M7743</guid>
      <dc:creator>Anandhu</dc:creator>
      <dc:date>2020-09-27T12:55:05Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1161638#M7762</link>
      <description>&lt;P&gt;Hi, &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65988"&gt;@Jonathan_Iglesias&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We were able to complete part 1 of "AuthenticateEV2First" using command :&lt;/P&gt;&lt;P&gt;&amp;nbsp;1.&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x90&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//cla&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x71&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//cmd&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//p1&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//p2&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x02&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//lc&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//key&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//lencap&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;//le&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;]&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;SPAN&gt;Authentication response : [147, 205, 124, 135, 153, 89, 104, 47, 41, 139, 13, 19, 29, 16, 52, 216, 145, 175].&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;We took Encrypted RndB as "147, 205, 124, 135, 153, 89, 104, 47, 41, 139, 13, 19, 29, 16, 52, 216" and tried to decrypt using key :&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;PRE&gt;{&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;&lt;SPAN&gt;, &lt;/SPAN&gt;&lt;SPAN&gt;0&lt;/SPAN&gt;} (0x00)&lt;/PRE&gt;&lt;SPAN&gt;&lt;SPAN&gt;but the response was "Pad block Corrupted".&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;SPAN&gt;Are we passing the right key?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&lt;SPAN&gt;Is there any other possibility of getting this error?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Thu, 01 Oct 2020 06:37:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1161638#M7762</guid>
      <dc:creator>Anandhu</dc:creator>
      <dc:date>2020-10-01T06:37:37Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1163484#M7775</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65988"&gt;@Jonathan_Iglesias&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for helping me to complete AuthenticateEV2First using APDU commands.&lt;/P&gt;&lt;P&gt;Now am trying to Get File Settings using this [CC file].&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="getFileSettings.PNG" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126814i8EF7BEA7DE2CD6C9/image-size/large?v=v2&amp;amp;px=999" role="button" title="getFileSettings.PNG" alt="getFileSettings.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;[&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x90&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0xf5&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x20&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x01&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;0x00&lt;/SPAN&gt;&lt;SPAN&gt;,&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;]&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;But the result is :&amp;nbsp;[145, 126] - Which is " LENGTH_ERROR 7Eh Command size not allowed."&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;Length will always be 1 byte. What will be the reason for this error.&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 06 Oct 2020 14:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1163484#M7775</guid>
      <dc:creator>Anandhu</dc:creator>
      <dc:date>2020-10-06T14:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: Ntag 424DNA write lock failed while using android Native method</title>
      <link>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1732461#M10800</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I know this question is from a long time ago. However, I am currently stuck at this step of writing on NTAG&amp;nbsp; 424 DNA. I would like to know if you have solved this problem. Additionally, I cannot convince myself to consider the 147, 205, 124, 135, 153, 89, 104, 47, 41, 139, 13, 19, 29, 16, 52, 216 as RndB . I think the result of E(k0 , RndB) should be equal to 147, 205, 124, 135, 153, 89, 104, 47, 41, 139, 13, 19, 29, 16, 52, 216.&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Mon, 02 Oct 2023 07:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Ntag-424DNA-write-lock-failed-while-using-android-Native-method/m-p/1732461#M10800</guid>
      <dc:creator>zahra2023</dc:creator>
      <dc:date>2023-10-02T07:42:01Z</dc:date>
    </item>
  </channel>
</rss>