<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [PN7462AU] ISO-DEP Protocol in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1156475#M7723</link>
    <description>&lt;P&gt;this is the ISO/IEC 14443-4 standard. This is fully supported. Device deactivation is the Deselect command. Also supported of course. Also higher abstractions like the ISO/IEC 7816-4 is supported.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In our PSP you will find plenty of examples using those mechanism to interact with cards. Like a DESFire for example&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&lt;/P&gt;</description>
    <pubDate>Mon, 21 Sep 2020 18:41:01 GMT</pubDate>
    <dc:creator>Jonathan_Iglesias</dc:creator>
    <dc:date>2020-09-21T18:41:01Z</dc:date>
    <item>
      <title>[PN7462AU] ISO-DEP Protocol</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1145580#M7654</link>
      <description>&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm a engineer using PN7462AU.&amp;nbsp;I am developing an NFC communication program.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Below is the setup details,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1. Hardware:&amp;nbsp;PN7462AU&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. SDK: PN7462AU-FW_v05.21.00&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. IDE: MCUXpresso IDE v11.0.0&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My question is about ISO-DEP Protocol. There is no mention of ISO-DEP in the PN7462AU SDK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 1) Is it correct that the PN7462AU SDK complies with the ISO-DEP protocol?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Since the ISO-DEP protocol is based on ISO/IEC 14443-4, there is no explicit word for ISO-DEP in the PN7462AU SDK, but the PN7462AU SDK complies with ISO/IEC 14443-4, so I think it also complies with the ISO-DEP protocol.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next question is below.&lt;/P&gt;&lt;P&gt;Device Deactivation is defined in the NFC Forum NFC activity specification.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 2) What API should be used in PN7462AU SDK to implement this Device Deactivation? Or is there a related example?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The phhalCt_CardActivate() and phhalCt_CardDeactivate() APIs are defined in phhalCt_Activate.c. Is it possible to implement Device Deactivation of NFC Forum Activity Specification by using this API?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If anyone knows the answer to your question, please reply.&lt;/P&gt;&lt;P&gt;If you have any question, please feel free to contact me.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Sep 2020 04:36:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1145580#M7654</guid>
      <dc:creator>autoever1leka</dc:creator>
      <dc:date>2020-09-04T04:36:01Z</dc:date>
    </item>
    <item>
      <title>Re: [PN7462AU] ISO-DEP Protocol</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1156475#M7723</link>
      <description>&lt;P&gt;this is the ISO/IEC 14443-4 standard. This is fully supported. Device deactivation is the Deselect command. Also supported of course. Also higher abstractions like the ISO/IEC 7816-4 is supported.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In our PSP you will find plenty of examples using those mechanism to interact with cards. Like a DESFire for example&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2020 18:41:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1156475#M7723</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-09-21T18:41:01Z</dc:date>
    </item>
    <item>
      <title>Re: [PN7462AU] ISO-DEP Protocol</title>
      <link>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1157587#M7730</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The NFC-DEP protocol is explicitly stated on the SDK, but ISO-DEP didn't come out so I asked.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;Thanks to you, the problem was solved, and what I wanted to check was confirmed. Thank you again sincerely.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 23 Sep 2020 08:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462AU-ISO-DEP-Protocol/m-p/1157587#M7730</guid>
      <dc:creator>autoever1leka</dc:creator>
      <dc:date>2020-09-23T08:21:55Z</dc:date>
    </item>
  </channel>
</rss>