<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Certification for PN532</title>
    <link>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1149378#M7643</link>
    <description>&lt;P&gt;is the PN532 allowed in the US? was also planning to design an RFID reader based on PN532 for door access but based on our research, 902~928MHz is the allowed frequency in the US. can PN532 is still be used which operates at 13.56MHz?&lt;/P&gt;</description>
    <pubDate>Mon, 07 Sep 2020 02:44:52 GMT</pubDate>
    <dc:creator>xt</dc:creator>
    <dc:date>2020-09-07T02:44:52Z</dc:date>
    <item>
      <title>Certification for PN532</title>
      <link>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1020275#M6795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My company has developed a product using PN532 chip and is now looking to get it certified (FCC and CE).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to our research we need to change the following parameters :&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Channel Selection&lt;/LI&gt;&lt;LI&gt;Continuous Transmission&lt;/LI&gt;&lt;LI&gt;Bit Rate Selection&lt;/LI&gt;&lt;LI&gt;Power Selection&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I read the datasheet could not find a way to change these parameters. Can anyone help me ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 07:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1020275#M6795</guid>
      <dc:creator>vaibhavchanana</dc:creator>
      <dc:date>2020-03-26T07:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: Certification for PN532</title>
      <link>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1020276#M6796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The information about the commands is available in the following App Note:&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf" title="https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf"&gt;https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please note that this is all the information we have at our reach since this device is not recommended for new designs. Thank you for your comprehension.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Mar 2020 20:44:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1020276#M6796</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-03-26T20:44:20Z</dc:date>
    </item>
    <item>
      <title>Re: Certification for PN532</title>
      <link>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1149378#M7643</link>
      <description>&lt;P&gt;is the PN532 allowed in the US? was also planning to design an RFID reader based on PN532 for door access but based on our research, 902~928MHz is the allowed frequency in the US. can PN532 is still be used which operates at 13.56MHz?&lt;/P&gt;</description>
      <pubDate>Mon, 07 Sep 2020 02:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Certification-for-PN532/m-p/1149378#M7643</guid>
      <dc:creator>xt</dc:creator>
      <dc:date>2020-09-07T02:44:52Z</dc:date>
    </item>
  </channel>
</rss>