<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NTAG emulation using NFC front-end</title>
    <link>https://community.nxp.com/t5/NFC/NTAG-emulation-using-NFC-front-end/m-p/1097910#M7613</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am developing my own NFC tag. At this stage I want to emulate the NTAG213 with custom hardware attached to it. &lt;BR /&gt;I have chosen the PN512 NFC front-end, which offers many opportunities for future development. Can you confirm, that:&lt;BR /&gt;-Is the PN512 capable of emulating NFC type 2 tag? In PNEV512B Quick Startup Guide there is only a T4T (tag type 4) example, in PN512 datasheet there is no info about, but there is a T2T example for the Raspberry PI (see AN11480).&lt;BR /&gt;-Does the PN512 in the card emulation mode work similar to NTAG I2C plus? Which one will be more suitable for a system with an MCU attached to the NFC part? Which one you suggest me to use?&amp;nbsp;&lt;/P&gt;&lt;P&gt;-I am right, that the NTAG I2C has the NFC stack already implemented, while the PN512 needs a custom stack implementation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Apr 2020 06:51:13 GMT</pubDate>
    <dc:creator>r_n123</dc:creator>
    <dc:date>2020-04-15T06:51:13Z</dc:date>
    <item>
      <title>NTAG emulation using NFC front-end</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-emulation-using-NFC-front-end/m-p/1097910#M7613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am developing my own NFC tag. At this stage I want to emulate the NTAG213 with custom hardware attached to it. &lt;BR /&gt;I have chosen the PN512 NFC front-end, which offers many opportunities for future development. Can you confirm, that:&lt;BR /&gt;-Is the PN512 capable of emulating NFC type 2 tag? In PNEV512B Quick Startup Guide there is only a T4T (tag type 4) example, in PN512 datasheet there is no info about, but there is a T2T example for the Raspberry PI (see AN11480).&lt;BR /&gt;-Does the PN512 in the card emulation mode work similar to NTAG I2C plus? Which one will be more suitable for a system with an MCU attached to the NFC part? Which one you suggest me to use?&amp;nbsp;&lt;/P&gt;&lt;P&gt;-I am right, that the NTAG I2C has the NFC stack already implemented, while the PN512 needs a custom stack implementation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2020 06:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-emulation-using-NFC-front-end/m-p/1097910#M7613</guid>
      <dc:creator>r_n123</dc:creator>
      <dc:date>2020-04-15T06:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: NTAG emulation using NFC front-end</title>
      <link>https://community.nxp.com/t5/NFC/NTAG-emulation-using-NFC-front-end/m-p/1097911#M7614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;-Is the PN512 capable of emulating NFC type 2 tag? In PNEV512B Quick Startup Guide there is only a T4T (tag type 4) example, in PN512 datasheet there is no info about, but there is a T2T example for the Raspberry PI (see AN11480).&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- Yes, it supports.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;BR /&gt;-Does the PN512 in the card emulation mode work similar to NTAG I2C plus? Which one will be more suitable for a system with an MCU attached to the NFC part? Which one you suggest me to use?&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- Yes, it does, but I would recommend using NTAG I2C directly if you just need functions of NTAG I2C.&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;-I am right, that the NTAG I2C has the NFC stack already implemented, while the PN512 needs a custom stack implementation?&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;- Actually NTAG I2C has all&amp;nbsp; functions implemented in its hardware, while PN512 still needs a software stack running on the host controller to behave as expected.&amp;nbsp;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2020 06:34:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NTAG-emulation-using-NFC-front-end/m-p/1097911#M7614</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-04-16T06:34:57Z</dc:date>
    </item>
  </channel>
</rss>