<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRATS and PPS code fails with Desfire EV2 cards - problem</title>
    <link>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094179#M7557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our product (Card Reader),&amp;nbsp; after many years of working fine with DESFire / DESFire EV1 cards,&amp;nbsp;is having&amp;nbsp;a problem when trying to interface DESFire EV2 cards, using the same program code that works well for all other DESfire cards.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My communication with the PICC fails in the ISO14443-4 part when using Desfire EV2 cards, in this procedure:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;I send RATS command "0xE0" with parameter 0x50&lt;/STRONG&gt; &lt;EM&gt;which corresponds to "FSDI defining maximum frame of bytes the PCD can receive" = 64. Also selects the CID (card identifier) to be = 0.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;- I receive 6 bytes response, assuming that it is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I sent the 3 bytes of &lt;STRONG&gt;PPS request&lt;/STRONG&gt; as follows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;0xD0&lt;/STRONG&gt; &lt;EM&gt;- the start byte,&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;0x11&lt;/STRONG&gt; &lt;EM&gt;- Parameter 0, indicates the presence of Parameter 1.&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;0x05&lt;/STRONG&gt; -&lt;EM&gt; Parameter 1, setting 212kbps for both DRI and DSI.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;After this, I get zero response from the PICC&lt;/STRONG&gt; where I should get the "0xD0" instead, and so afterward's no communication is available with the PICC &lt;STRONG&gt;so this is the fail part!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The same code works fine for all DESFire cards except Desfire EV2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The used frontend chip is &lt;STRONG&gt;MFRC522&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What might be the problem? Why would EV2 fail way back in the&amp;nbsp;I&lt;SPAN&gt;SO14443-4 part where other cards work fine?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Apr 2020 08:40:15 GMT</pubDate>
    <dc:creator>spasovski_dejan</dc:creator>
    <dc:date>2020-04-29T08:40:15Z</dc:date>
    <item>
      <title>RATS and PPS code fails with Desfire EV2 cards - problem</title>
      <link>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094179#M7557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our product (Card Reader),&amp;nbsp; after many years of working fine with DESFire / DESFire EV1 cards,&amp;nbsp;is having&amp;nbsp;a problem when trying to interface DESFire EV2 cards, using the same program code that works well for all other DESfire cards.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;My communication with the PICC fails in the ISO14443-4 part when using Desfire EV2 cards, in this procedure:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- &lt;STRONG&gt;I send RATS command "0xE0" with parameter 0x50&lt;/STRONG&gt; &lt;EM&gt;which corresponds to "FSDI defining maximum frame of bytes the PCD can receive" = 64. Also selects the CID (card identifier) to be = 0.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;- I receive 6 bytes response, assuming that it is OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I sent the 3 bytes of &lt;STRONG&gt;PPS request&lt;/STRONG&gt; as follows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;0xD0&lt;/STRONG&gt; &lt;EM&gt;- the start byte,&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;0x11&lt;/STRONG&gt; &lt;EM&gt;- Parameter 0, indicates the presence of Parameter 1.&lt;/EM&gt;&lt;BR /&gt;&lt;STRONG&gt;0x05&lt;/STRONG&gt; -&lt;EM&gt; Parameter 1, setting 212kbps for both DRI and DSI.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;After this, I get zero response from the PICC&lt;/STRONG&gt; where I should get the "0xD0" instead, and so afterward's no communication is available with the PICC &lt;STRONG&gt;so this is the fail part!&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The same code works fine for all DESFire cards except Desfire EV2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The used frontend chip is &lt;STRONG&gt;MFRC522&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;What might be the problem? Why would EV2 fail way back in the&amp;nbsp;I&lt;SPAN&gt;SO14443-4 part where other cards work fine?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 08:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094179#M7557</guid>
      <dc:creator>spasovski_dejan</dc:creator>
      <dc:date>2020-04-29T08:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: RATS and PPS code fails with Desfire EV2 cards - problem</title>
      <link>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094180#M7558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are doing well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As you might know, there are some of the documents and libraries which are under NDA (Non-Disclosure Agreement), the DESFIRE information is under NDA and the information can't be shared in a public way. Sorry for the inconvenience this might cause you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 18:52:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094180#M7558</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-04-29T18:52:10Z</dc:date>
    </item>
    <item>
      <title>Re: RATS and PPS code fails with Desfire EV2 cards - problem</title>
      <link>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094181#M7559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo,&lt;BR /&gt;&lt;BR /&gt;Thanks for your fast reply! Our company already has signed the NDA so if you can please refer to what document should I download from docstore regarding this issue?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Apr 2020 19:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094181#M7559</guid>
      <dc:creator>spasovski_dejan</dc:creator>
      <dc:date>2020-04-29T19:37:01Z</dc:date>
    </item>
    <item>
      <title>Re: RATS and PPS code fails with Desfire EV2 cards - problem</title>
      <link>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094182#M7560</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Dejan,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I replied in a private message.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2020 22:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RATS-and-PPS-code-fails-with-Desfire-EV2-cards-problem/m-p/1094182#M7560</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-04-30T22:31:18Z</dc:date>
    </item>
  </channel>
</rss>