<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7150 Type 4 card emulation with RPi/Python in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7150-Type-4-card-emulation-with-RPi-Python/m-p/1085796#M7466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may refer to this :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11990.pdf" title="https://www.nxp.com/docs/en/application-note/AN11990.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11990.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;H3 class=""&gt;&lt;A class="" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="NXP-NCI MCUXpresso example Project " href="https://www.nxp.com/webapp/Download?colCode=SW4325&amp;amp;appType=license"&gt;NXP-NCI MCUXpresso example Project&lt;/A&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Aug 2020 04:45:38 GMT</pubDate>
    <dc:creator>jimmychan</dc:creator>
    <dc:date>2020-08-24T04:45:38Z</dc:date>
    <item>
      <title>PN7150 Type 4 card emulation with RPi/Python</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Type-4-card-emulation-with-RPi-Python/m-p/1085795#M7465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello NXP community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am at a beginner level in both programming hardware and NFC, so please excuse any incorrect terminology I use. I have a PN7150 on a OM5578 kit on a Raspberry Pi 4. My ultimate goal is to write Python script that will write text&amp;nbsp;onto the NFC card&amp;nbsp;and do Type 4 Card emulation so that I can transfer that text to an NFC reader device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like the nfcDemoApp does not support Type 4 Card emulation, so I am wondering if there are any resources I can be directed to that will allow me to test out Type 4 Card emulation capabilities of the PN7150/OM5578 on the Raspberry Pi.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From my search online, there does not seem to be any Raspberry Pi/Python Type 4 Card emulation support for the PN7150. Although I can find some C and C++ resources for the PN532 or PN7120, I read that those resources do not support PN7150 and those models interface&amp;nbsp;on the SPI bus instead of the I2C bus.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I could get some help interfacing the PN7150 via I2C bus on the Raspberry Pi 4 (using Python) to write data onto the PN7150 and emulate a Type 4 card (ISO/IEC 14443 A and/or B), that would be VERY helpful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/nfc pn7510/tg-p"&gt;#nfc pn7510&lt;/A&gt;&amp;nbsp;pn7150‌ &lt;A href="https://community.nxp.com/t5/tag/pn7150rpi/tg-p"&gt;#pn7150rpi&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/card emulation/tg-p"&gt;#card emulation&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/iso1443 4/3 type a and b/tg-p"&gt;#iso1443 4/3 type a and b&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/i2c protocol/tg-p"&gt;#i2c protocol&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/raspberrypi/tg-p"&gt;#raspberrypi&lt;/A&gt;‌ &lt;A href="https://community.nxp.com/t5/tag/nfc om5578/tg-p"&gt;#nfc om5578&lt;/A&gt;‌ #nfc&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2020 16:30:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Type-4-card-emulation-with-RPi-Python/m-p/1085795#M7465</guid>
      <dc:creator>david_nash</dc:creator>
      <dc:date>2020-08-12T16:30:54Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Type 4 card emulation with RPi/Python</title>
      <link>https://community.nxp.com/t5/NFC/PN7150-Type-4-card-emulation-with-RPi-Python/m-p/1085796#M7466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You may refer to this :&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11990.pdf" title="https://www.nxp.com/docs/en/application-note/AN11990.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11990.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;H3 class=""&gt;&lt;A class="" data-dtmaction="Documents and Software Results - Software Link click" data-dtmsubaction="NXP-NCI MCUXpresso example Project " href="https://www.nxp.com/webapp/Download?colCode=SW4325&amp;amp;appType=license"&gt;NXP-NCI MCUXpresso example Project&lt;/A&gt;&lt;/H3&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Aug 2020 04:45:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7150-Type-4-card-emulation-with-RPi-Python/m-p/1085796#M7466</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2020-08-24T04:45:38Z</dc:date>
    </item>
  </channel>
</rss>