<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: CLRC663 Interrupt</title>
    <link>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083262#M7462</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the explanation, I believe the IRQ1En options are the only one available for IRQ1 interrupt requests e.g., to set the pin as push-pull or open-drain, whilst the inverted functionality is only available for IRQ0 interrupt sources in IQ0En.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jun 2020 19:09:45 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2020-06-05T19:09:45Z</dc:date>
    <item>
      <title>CLRC663 Interrupt</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083259#M7459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm testing the CLRC663's LPCD feature without&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;NFC Reader Library on&amp;nbsp;&lt;SPAN style="color: #333f48; font-size: 16px;"&gt;CLEV6630B board&lt;/SPAN&gt; .&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Now I can read the UID of tag and can implement LPCD successfully.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;But I face a problem when test the interrupt request from&amp;nbsp;&lt;SPAN style="color: #3d3d3d;"&gt;CLRC663.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I don't know why the voltage leve of &lt;SPAN style="color: #3d3d3d;"&gt;CLRC663&amp;nbsp; IRQ pin change from high to low level after set the&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;IRQ0En register and&amp;nbsp;enable the interrupt.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;May I have information for the&amp;nbsp;timing diagram of C&lt;SPAN style="color: #3d3d3d;"&gt;RC663 &lt;SPAN style="background-color: #ffffff;"&gt;IRQ pin&lt;/SPAN&gt;?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;And when I need to set this IRQ_Inv bit (Set to one the signal of the IRQ pin is inverted) in&amp;nbsp;IRQ0En register?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thank so much for your advice.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 06:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083259#M7459</guid>
      <dc:creator>breezeto</dc:creator>
      <dc:date>2020-05-28T06:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Interrupt</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083260#M7460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;May I ask which value you are loading to IRQ0En?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2020 22:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083260#M7460</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-06-03T22:21:22Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Interrupt</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083261#M7461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ivan&lt;/P&gt;&lt;P&gt;The value of IRQ0En register is loaded 0x80, I only set the IRQ_Inv bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At beginning the voltage level of&amp;nbsp;IRQ Pin&amp;nbsp;is high level. It&amp;nbsp;will become&amp;nbsp;to low level when I enable the Timer3 interrupt request on the IRQ1ENn register and the timer3 has an underflow.&lt;/P&gt;&lt;P&gt;But the voltage level of&lt;SPAN&gt;&amp;nbsp;IRQ Pin will not change to&amp;nbsp;high level even I clear the IRQ0 &amp;amp; IRQ1 register (load 0x7F, 0x7F).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I'm not sure does it correct. Or I made any mistake.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks~&lt;/P&gt;&lt;P&gt;Breeze&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2020 02:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083261#M7461</guid>
      <dc:creator>breezeto</dc:creator>
      <dc:date>2020-06-04T02:13:12Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Interrupt</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083262#M7462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the explanation, I believe the IRQ1En options are the only one available for IRQ1 interrupt requests e.g., to set the pin as push-pull or open-drain, whilst the inverted functionality is only available for IRQ0 interrupt sources in IQ0En.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2020 19:09:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1083262#M7462</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-06-05T19:09:45Z</dc:date>
    </item>
    <item>
      <title>Re: CLRC663 Interrupt</title>
      <link>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1575399#M9915</link>
      <description>&lt;P&gt;I facing this problem also. seem like the IRQ always low will enable&amp;nbsp;IRQPinEn bit. Another question is when any interrupt occur the IRQ pin is rising edge or falling edge? and the hold time is how long?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 04:14:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/CLRC663-Interrupt/m-p/1575399#M9915</guid>
      <dc:creator>CBLeong</dc:creator>
      <dc:date>2022-12-29T04:14:46Z</dc:date>
    </item>
  </channel>
</rss>