<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI slave mode selection And SPI send function does not work in NFC</title>
    <link>https://community.nxp.com/t5/NFC/SPI-slave-mode-selection-And-SPI-send-function-does-not-work/m-p/1081208#M7428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A related question was already asked in following community thread, please help us to refer to it:&amp;nbsp;&lt;A href="https://community.nxp.com/message/1047051"&gt;https://community.nxp.com/message/1047051&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Apr 2020 20:21:39 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2020-04-27T20:21:39Z</dc:date>
    <item>
      <title>SPI slave mode selection And SPI send function does not work</title>
      <link>https://community.nxp.com/t5/NFC/SPI-slave-mode-selection-And-SPI-send-function-does-not-work/m-p/1081207#M7427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello there! How can I set the PN7462 to work in HDLL mode, NATIVE mode or NCI mode during the use of PN7462 as SPI communication slave?&lt;BR /&gt;When I set PN7462 as SPI slave, use the following statement re = phhalHif_Transmit ((uint32_t *) &amp;amp; temp, 8, (pphhalHif_Callback_t) &amp;amp; phExPos_SPIHIFSPITxCallback); When the function sends data 0x10005105, MISO is always high. The return value of phhalHif_Transmit is 0, that is, re = 0.&lt;BR /&gt;But when I let the phhalHif_Transmit function execute cyclically, the code can be sent normally as follows&lt;/P&gt;&lt;P&gt;while (1) {&lt;BR /&gt;&amp;nbsp; re = phhalHif_Transmit ((uint32_t *) &amp;amp; temp, 8, (pphhalHif_Callback_t) &amp;amp; phExPos_SPIHIFSPITxCallback);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;May I ask why?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2020 03:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/SPI-slave-mode-selection-And-SPI-send-function-does-not-work/m-p/1081207#M7427</guid>
      <dc:creator>15041539</dc:creator>
      <dc:date>2020-04-27T03:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: SPI slave mode selection And SPI send function does not work</title>
      <link>https://community.nxp.com/t5/NFC/SPI-slave-mode-selection-And-SPI-send-function-does-not-work/m-p/1081208#M7428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A related question was already asked in following community thread, please help us to refer to it:&amp;nbsp;&lt;A href="https://community.nxp.com/message/1047051"&gt;https://community.nxp.com/message/1047051&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Apr 2020 20:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/SPI-slave-mode-selection-And-SPI-send-function-does-not-work/m-p/1081208#M7428</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-04-27T20:21:39Z</dc:date>
    </item>
  </channel>
</rss>