<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NFC: Rmatch value for matching circuit in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077477#M7381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi Asael,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Actually the matching process is almost the same, while the target impedance depends on&amp;nbsp;&lt;SPAN&gt;the NFC controller chosen.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 May 2020 09:12:32 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2020-05-20T09:12:32Z</dc:date>
    <item>
      <title>NFC: Rmatch value for matching circuit</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077474#M7378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing the NFC antenna and using PN532 NFC controller for a project. I'm not a expert about NFC or RF circuits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some questions about Rmatch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About Rmatch I understand that need to be measure with an impedance or network analyzer. But, for prototype design, with what value of Rmatch I can obtain values for matching? &lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;What value of Rmatch should I start with?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there only a Rmatch = 50 Ohms or is there a range?&lt;/P&gt;&lt;P&gt;If there is a range, what is the range?, and, how affect &lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;a greater or lesser value of Rmatch to the NFC circuit?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;SPAN class="" title=""&gt;Thanks for your replies&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 15:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077474#M7378</guid>
      <dc:creator>asael_hernandez</dc:creator>
      <dc:date>2020-05-12T15:16:18Z</dc:date>
    </item>
    <item>
      <title>Re: NFC: Rmatch value for matching circuit</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077475#M7379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Asael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, for PN532, the recommended Rmatch is around 50ohm, and the range is&amp;nbsp;40 - 50 Ohm, the general tuning flow is like below, and please kindly refer to&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN1445_An1444.zip" title="https://www.nxp.com/docs/en/application-note/AN1445_An1444.zip"&gt;https://www.nxp.com/docs/en/application-note/AN1445_An1444.zip&lt;/A&gt;&amp;nbsp; for more details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107767i6D589FB503BC0F9D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 02:51:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077475#M7379</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-05-15T02:51:31Z</dc:date>
    </item>
    <item>
      <title>Re: NFC: Rmatch value for matching circuit</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077476#M7380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more question. The impedance matching depends only on the NFC controller chosen? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 00:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077476#M7380</guid>
      <dc:creator>asael_hernandez</dc:creator>
      <dc:date>2020-05-20T00:51:00Z</dc:date>
    </item>
    <item>
      <title>Re: NFC: Rmatch value for matching circuit</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077477#M7381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi Asael,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Actually the matching process is almost the same, while the target impedance depends on&amp;nbsp;&lt;SPAN&gt;the NFC controller chosen.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P style="background-color: #ffffff; border: 0px;"&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 09:12:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1077477#M7381</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-05-20T09:12:32Z</dc:date>
    </item>
    <item>
      <title>Re: NFC: Rmatch value for matching circuit</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1449915#M9401</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I am using a PN7150 in reader mode. Matching is done according to the application note right up to the RX path.&lt;/P&gt;&lt;P&gt;What I've seen is, that some NFC Tags have an extensive impact on our antenna characteristics.&amp;nbsp; This means that although our circuit is matched for unaffected scenario (and some smaller 15693 Tags), all 14443 tags I've tested made it perform considerably worse. When you look at a typical smith chart measured at both TX pins, the presence of an 14443 tag throws the 13.56MHz mark right down to the low resistance area (talking R&amp;lt;10ohm for a Z(Rmatch) = 40ohm circuit). This will increase current consumption for the duration and probably decreases EMC compliance.&amp;nbsp;&lt;BR /&gt;How should we handle that? Problem is, that we use both types of tags and have to pass booth EMC tests.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Apr 2022 12:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Rmatch-value-for-matching-circuit/m-p/1449915#M9401</guid>
      <dc:creator>Gladiator13</dc:creator>
      <dc:date>2022-04-27T12:21:11Z</dc:date>
    </item>
  </channel>
</rss>