<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Why is &amp;quot;LAST_NDEF_BLOCK&amp;quot; always zero in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067676#M7292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;LAST_NDEF_BLOCK works as “monitor” which can be set to monitor a change of value in chosen UserMemory block. When value in that block changes, ED (interrupt) is fired.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please could you explain how this is done, both from I2C perspective and NFC perspective. I had somehow assumed that this was automatic and I did not realise it can be used to monitor a chosen UserMemory block, which is quite useful.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 May 2020 09:54:49 GMT</pubDate>
    <dc:creator>gerrikoio</dc:creator>
    <dc:date>2020-05-15T09:54:49Z</dc:date>
    <item>
      <title>Why is "LAST_NDEF_BLOCK" always zero</title>
      <link>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067673#M7289</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently got some PCB's made and populated these with some NT3H2111 and NT3H2211 NTAG I2C plus tags.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NFC read and write from a phone using the various NXP NFC apps, such as TagWriter, TagInfo and NTAG I2C demo all work fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However with the TagInfo app, in EXTRA, it tells me that my last NDEF message page address has an error as this is 0x00.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I read the capability container from I2C it confirms this too.&amp;nbsp;LAST_NDEF_BLOCK: 0x00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can still read/write NDEF message using the apps, but I cannot read these NDEF messages from I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is this normal with unconfigured&amp;nbsp;NT3H2111/NT3H2211&amp;nbsp;tags?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN&gt;Or, are there certain things I need to do to get these tags "ready" so that I can read/write from I2C and also ensure that the&amp;nbsp;LAST_NDEF_BLOCK is correct.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;So, for example, what do I do with&amp;nbsp;&lt;SPAN&gt;LAST_NDEF_BLOCK. Do I have to manually set this to 0x01 before use?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 May 2020 19:29:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067673#M7289</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2020-05-09T19:29:11Z</dc:date>
    </item>
    <item>
      <title>Re: Why is "LAST_NDEF_BLOCK" always zero</title>
      <link>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067674#M7290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry I meant Session Registers not Capability Container for the byte&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;LAST_NDEF_BLOCK which is set to 0x00 (default)&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 09 May 2020 21:02:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067674#M7290</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2020-05-09T21:02:27Z</dc:date>
    </item>
    <item>
      <title>Re: Why is "LAST_NDEF_BLOCK" always zero</title>
      <link>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067675#M7291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="337920" data-username="gerrikoio" href="https://community.nxp.com/people/gerrikoio"&gt;Colin Gerrish&lt;/A&gt;&lt;/P&gt;&lt;P&gt;LAST_NDEF_BLOCK works as “monitor” which can be set to monitor a change of value in chosen UserMemory block. When value in that block changes, ED (interrupt) is fired. E.g. This can notify µC that it can start accessing eeprom.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;User Memory can always be read by I²C if I2C_PROT is not 1b. Beware to use proper command formatting on i²C which differs from register access formatting, described on page 44 of Datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/107289iE2778532F210543B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 May 2020 21:24:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067675#M7291</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-05-13T21:24:32Z</dc:date>
    </item>
    <item>
      <title>Re: Why is "LAST_NDEF_BLOCK" always zero</title>
      <link>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067676#M7292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;LAST_NDEF_BLOCK works as “monitor” which can be set to monitor a change of value in chosen UserMemory block. When value in that block changes, ED (interrupt) is fired.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please could you explain how this is done, both from I2C perspective and NFC perspective. I had somehow assumed that this was automatic and I did not realise it can be used to monitor a chosen UserMemory block, which is quite useful.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 May 2020 09:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067676#M7292</guid>
      <dc:creator>gerrikoio</dc:creator>
      <dc:date>2020-05-15T09:54:49Z</dc:date>
    </item>
    <item>
      <title>Re: Why is "LAST_NDEF_BLOCK" always zero</title>
      <link>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067677#M7293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check the DS&amp;nbsp;&lt;/P&gt;&lt;P&gt;there is an explanation of it in table 13. please check it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/108494iECFA314B7EEACB1A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf?pspll=1" title="https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf?pspll=1"&gt;https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf?pspll=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2020 21:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Why-is-quot-LAST-NDEF-BLOCK-quot-always-zero/m-p/1067677#M7293</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-05-28T21:22:49Z</dc:date>
    </item>
  </channel>
</rss>