<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN5180 Card emulation function question in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN5180-Card-emulation-function-question/m-p/1060582#M7169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;Hi.&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;The card emulation function of PN5180 is review.&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;Regarding the iPhone and card emulation function,&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;The iPhone is a card reader, and the application with PN5180 can communicate with the iPhone through Felica type, and I would like to ask if it is possible to process it in F/W with a specific data value.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Jul 2020 05:04:43 GMT</pubDate>
    <dc:creator>chlee2</dc:creator>
    <dc:date>2020-07-03T05:04:43Z</dc:date>
    <item>
      <title>PN5180 Card emulation function question</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Card-emulation-function-question/m-p/1060582#M7169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;Hi.&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;The card emulation function of PN5180 is review.&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;Regarding the iPhone and card emulation function,&lt;/SPAN&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;BR style="color: #000000; background-color: #fdfdfd;" /&gt;&lt;SPAN style="color: #000000; background-color: #fdfdfd;"&gt;The iPhone is a card reader, and the application with PN5180 can communicate with the iPhone through Felica type, and I would like to ask if it is possible to process it in F/W with a specific data value.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2020 05:04:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Card-emulation-function-question/m-p/1060582#M7169</guid>
      <dc:creator>chlee2</dc:creator>
      <dc:date>2020-07-03T05:04:43Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180 Card emulation function question</title>
      <link>https://community.nxp.com/t5/NFC/PN5180-Card-emulation-function-question/m-p/1060583#M7170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PN5180 frontend IC supports the following RF operating modes:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;• Reader/Writer mode supporting ISO/IEC 14443 type A up to 848 kBit/s&lt;BR /&gt;• Reader/Writer communication mode for MIFARE Classic contactless IC&lt;BR /&gt;• Reader/Writer mode supporting ISO/IEC 14443 type B up to 848 kBit/s&lt;BR /&gt;• Reader/Writer mode supporting JIS X 6319-4 (comparable with FeliCa scheme)&lt;BR /&gt;• Supports reading of all NFC tag types (type 1, type 2, type 3, type 4A and type 4B)&lt;BR /&gt;• Reader/Writer mode supporting ISO/IEC 15693&lt;BR /&gt;• Reader/Writer mode supporting ISO/IEC 18000-3 Mode 3&lt;BR /&gt;• ISO/IEC 18092 (NFC-IP1)&lt;BR /&gt;• ISO/IEC 21481 (NFC-IP-2)&lt;BR /&gt;• ISO/IEC 14443 type A Card emulation up to 848 kBit/s&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check more details about this in the &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/full-nfc-forum-compliant-frontend-ic:PN5180?tab=Documentation_Tab&amp;amp;linkline=Data%20Sheet&amp;amp;fpsp=1"&gt;Datasheet &lt;/A&gt;of the device. The device does not list the Felica Type in the card emulation mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can emulate a type A card and read it with the phone.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Jul 2020 18:54:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN5180-Card-emulation-function-question/m-p/1060583#M7170</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2020-07-07T18:54:49Z</dc:date>
    </item>
  </channel>
</rss>