<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AN10834 - How to Make MIFARE Plus give RATS on SL1? in NFC</title>
    <link>https://community.nxp.com/t5/NFC/AN10834-How-to-Make-MIFARE-Plus-give-RATS-on-SL1/m-p/1052104#M7101</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SAK for Mifare Plus in SL1 is 0x08 or 0x18.&amp;nbsp; That doesn't include bit 6 (0x20) indicating ISO 14443-4 Compliance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thus when using&amp;nbsp;&lt;SPAN class=""&gt;NxpNfcRdLib, it will not automatically query for RATS/ATS response when seeing a MFPlusX in SL1 Mifare Classic Emulation Mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So I tried to manually use&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;phpalI14443p4a_Rats anyways, but get back error status =&amp;nbsp; 0x0502&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;PH_COMP_PAL_ISO14443P4A/PH_ERR_INVALID_DATA_PARAMS&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Anyways, I have a feeling it's not possible to get historical bytes in SL1.&amp;nbsp; Great emulation of MF Classic 1K though.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;If that's the case, how can to detect that a card is MF Plus in SL1 mode without RATS/Historical Bytes?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(RATS/ATS in SL0's SAK=0x20 works great so I know I'm doing something right)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I was thinking of using the Originality Key, but there's no application note on&amp;nbsp;the NDA Site for MF Plus S/X related to that.&amp;nbsp; &amp;nbsp;It's missing from the API of the NxpNfcRdLib as well for phalMfp.&amp;nbsp; &amp;nbsp;Maybe pdf/api needs to be uploaded?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 19 Apr 2020 20:27:48 GMT</pubDate>
    <dc:creator>eljeffo</dc:creator>
    <dc:date>2020-04-19T20:27:48Z</dc:date>
    <item>
      <title>AN10834 - How to Make MIFARE Plus give RATS on SL1?</title>
      <link>https://community.nxp.com/t5/NFC/AN10834-How-to-Make-MIFARE-Plus-give-RATS-on-SL1/m-p/1052104#M7101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SAK for Mifare Plus in SL1 is 0x08 or 0x18.&amp;nbsp; That doesn't include bit 6 (0x20) indicating ISO 14443-4 Compliance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thus when using&amp;nbsp;&lt;SPAN class=""&gt;NxpNfcRdLib, it will not automatically query for RATS/ATS response when seeing a MFPlusX in SL1 Mifare Classic Emulation Mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;So I tried to manually use&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN class=""&gt;phpalI14443p4a_Rats anyways, but get back error status =&amp;nbsp; 0x0502&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;PH_COMP_PAL_ISO14443P4A/PH_ERR_INVALID_DATA_PARAMS&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Anyways, I have a feeling it's not possible to get historical bytes in SL1.&amp;nbsp; Great emulation of MF Classic 1K though.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;If that's the case, how can to detect that a card is MF Plus in SL1 mode without RATS/Historical Bytes?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;(RATS/ATS in SL0's SAK=0x20 works great so I know I'm doing something right)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;I was thinking of using the Originality Key, but there's no application note on&amp;nbsp;the NDA Site for MF Plus S/X related to that.&amp;nbsp; &amp;nbsp;It's missing from the API of the NxpNfcRdLib as well for phalMfp.&amp;nbsp; &amp;nbsp;Maybe pdf/api needs to be uploaded?&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Apr 2020 20:27:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/AN10834-How-to-Make-MIFARE-Plus-give-RATS-on-SL1/m-p/1052104#M7101</guid>
      <dc:creator>eljeffo</dc:creator>
      <dc:date>2020-04-19T20:27:48Z</dc:date>
    </item>
    <item>
      <title>Re: AN10834 - How to Make MIFARE Plus give RATS on SL1?</title>
      <link>https://community.nxp.com/t5/NFC/AN10834-How-to-Make-MIFARE-Plus-give-RATS-on-SL1/m-p/1052105#M7102</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Nevermind, just force 14443-4 activation...but... how to do that formally?&amp;nbsp; Check this next thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/530328"&gt;https://community.nxp.com/thread/530328&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2020 22:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/AN10834-How-to-Make-MIFARE-Plus-give-RATS-on-SL1/m-p/1052105#M7102</guid>
      <dc:creator>eljeffo</dc:creator>
      <dc:date>2020-04-20T22:09:44Z</dc:date>
    </item>
  </channel>
</rss>