<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: Application Identifiers to add in info.plist (Swift iOS programming) for MIFARE</title>
    <link>https://community.nxp.com/t5/NFC/Application-Identifiers-to-add-in-info-plist-Swift-iOS/m-p/1050421#M7100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="360739" data-username="heinimueller@tm.in-ulm.de" href="https://community.nxp.com/people/heinimueller@tm.in-ulm.de"&gt;Heini Müller&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great, as you may know IOS supports the NDEF interaction,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-with-ios-13-:NFC_IOS_13" title="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-with-ios-13-:NFC_IOS_13"&gt;Unleash the full potential of NFC with iOS 13 and NXP | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not sure if you mean the DF names and the file IDs, as you may know when you have a type 4 tag there is a certain file structure to comply with the 7816-4&amp;nbsp; please check for example our NTAG 424&amp;nbsp; which has preloaded this type of structure for more information please check the ISO 7816-4 spec&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/113464i4853DB0A65BADADB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jun 2020 19:55:45 GMT</pubDate>
    <dc:creator>Jonathan_Iglesias</dc:creator>
    <dc:date>2020-06-22T19:55:45Z</dc:date>
    <item>
      <title>Application Identifiers to add in info.plist (Swift iOS programming) for MIFARE</title>
      <link>https://community.nxp.com/t5/NFC/Application-Identifiers-to-add-in-info-plist-Swift-iOS/m-p/1050420#M7099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to add Mifare support for my iOS app and ran into some problems. Concretely I would like to read the Mifare-Card's UID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I got, I need to pass some "Application Identifiers" (AID?) into the info.plist to get the tagReaderSession to callback. What is / are the AIDs for Mifare classic 1K, Mifare Classic 4K, Mifare Plus EV1, Mifare Ultralight EV1, Mifare Desfire EV1 and Mifare Plus EV1?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would be very happy about any kind of help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2020 06:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Application-Identifiers-to-add-in-info-plist-Swift-iOS/m-p/1050420#M7099</guid>
      <dc:creator>heinimueller</dc:creator>
      <dc:date>2020-06-16T06:40:32Z</dc:date>
    </item>
    <item>
      <title>Re: Application Identifiers to add in info.plist (Swift iOS programming) for MIFARE</title>
      <link>https://community.nxp.com/t5/NFC/Application-Identifiers-to-add-in-info-plist-Swift-iOS/m-p/1050421#M7100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="360739" data-username="heinimueller@tm.in-ulm.de" href="https://community.nxp.com/people/heinimueller@tm.in-ulm.de"&gt;Heini Müller&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great, as you may know IOS supports the NDEF interaction,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-with-ios-13-:NFC_IOS_13" title="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-with-ios-13-:NFC_IOS_13"&gt;Unleash the full potential of NFC with iOS 13 and NXP | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am not sure if you mean the DF names and the file IDs, as you may know when you have a type 4 tag there is a certain file structure to comply with the 7816-4&amp;nbsp; please check for example our NTAG 424&amp;nbsp; which has preloaded this type of structure for more information please check the ISO 7816-4 spec&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/113464i4853DB0A65BADADB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jun 2020 19:55:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Application-Identifiers-to-add-in-info-plist-Swift-iOS/m-p/1050421#M7100</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-06-22T19:55:45Z</dc:date>
    </item>
  </channel>
</rss>