<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: PNEV5180B with external MCU</title>
    <link>https://community.nxp.com/t5/NFC/PNEV5180B-with-external-MCU/m-p/1044542#M7012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bryan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to "5.2 Connecting the FRDM-K82F to the PNEV5180B" in the following links:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11908.pdf" title="https://www.nxp.com/docs/en/application-note/AN11908.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11908.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The steps can also be applied for any other external MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Apr 2020 03:34:00 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2020-04-17T03:34:00Z</dc:date>
    <item>
      <title>PNEV5180B with external MCU</title>
      <link>https://community.nxp.com/t5/NFC/PNEV5180B-with-external-MCU/m-p/1044541#M7011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm starting to use the&amp;nbsp;PNEV5180B dev kit and would like to interface it with an external MCU. Do I need to/how can I bypass the connections of the PN5180 with the LPC1769 and just jump the connections to my external board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2020 18:22:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PNEV5180B-with-external-MCU/m-p/1044541#M7011</guid>
      <dc:creator>bryan3</dc:creator>
      <dc:date>2020-04-16T18:22:57Z</dc:date>
    </item>
    <item>
      <title>Re: PNEV5180B with external MCU</title>
      <link>https://community.nxp.com/t5/NFC/PNEV5180B-with-external-MCU/m-p/1044542#M7012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bryan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to "5.2 Connecting the FRDM-K82F to the PNEV5180B" in the following links:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN11908.pdf" title="https://www.nxp.com/docs/en/application-note/AN11908.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11908.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The steps can also be applied for any other external MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Apr 2020 03:34:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PNEV5180B-with-external-MCU/m-p/1044542#M7012</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-04-17T03:34:00Z</dc:date>
    </item>
  </channel>
</rss>