<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Re: 66301 Chip question</title>
    <link>https://community.nxp.com/t5/NFC/66301-Chip-question/m-p/1042704#M6988</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is also CLRC663, but not plus version, the plus is CLRC66303,&amp;nbsp; and it provides the following features comparing with CLRC663:&lt;/P&gt;&lt;P&gt;--Provides larger temperature range.&lt;BR /&gt;--Provides higher ITVDD range.&lt;BR /&gt;--Provides improved LPCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and they are pin to pin compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that makes sense,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 Apr 2020 03:40:32 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2020-04-17T03:40:32Z</dc:date>
    <item>
      <title>66301 Chip question</title>
      <link>https://community.nxp.com/t5/NFC/66301-Chip-question/m-p/1042703#M6987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking to understand exactly what chip this is and if it is the same class as the CLRC633.&amp;nbsp; What are the differences?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2020 18:06:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/66301-Chip-question/m-p/1042703#M6987</guid>
      <dc:creator>eric4</dc:creator>
      <dc:date>2020-04-16T18:06:33Z</dc:date>
    </item>
    <item>
      <title>Re: 66301 Chip question</title>
      <link>https://community.nxp.com/t5/NFC/66301-Chip-question/m-p/1042704#M6988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, it is also CLRC663, but not plus version, the plus is CLRC66303,&amp;nbsp; and it provides the following features comparing with CLRC663:&lt;/P&gt;&lt;P&gt;--Provides larger temperature range.&lt;BR /&gt;--Provides higher ITVDD range.&lt;BR /&gt;--Provides improved LPCD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and they are pin to pin compatible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that makes sense,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Apr 2020 03:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/66301-Chip-question/m-p/1042704#M6988</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2020-04-17T03:40:32Z</dc:date>
    </item>
  </channel>
</rss>