<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  NT3H2111 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1039450#M6956</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You probably enabled the NFC silent mode in NC_REG, so the NFC reader cannot "see" the NTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this should be able to change back from I2C interface. Did you use the correct I2C command? There are different commands for I2C register read/write and I2C data read/write.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Jul 2020 02:12:18 GMT</pubDate>
    <dc:creator>Xiang_Li</dc:creator>
    <dc:date>2020-07-30T02:12:18Z</dc:date>
    <item>
      <title>NT3H2111</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1039449#M6955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We mistakenly wrote Configuration register NC_REG as 0xFD during development&lt;/P&gt;&lt;P&gt;At present, I put NT3H2111 on the NFC card reader, and the card reader cannot connect the NFC Tag. At this time, the NC_REG value of the Configuration registers read from the i2c is 0xFD, and its content cannot be cleared&lt;/P&gt;&lt;P&gt;Excuse me, how to change the value of NC_REG to 0x01 from i2c?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tein&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2020 01:40:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1039449#M6955</guid>
      <dc:creator>teinsu</dc:creator>
      <dc:date>2020-07-30T01:40:03Z</dc:date>
    </item>
    <item>
      <title>Re:  NT3H2111</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1039450#M6956</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You probably enabled the NFC silent mode in NC_REG, so the NFC reader cannot "see" the NTAG.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this should be able to change back from I2C interface. Did you use the correct I2C command? There are different commands for I2C register read/write and I2C data read/write.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2020 02:12:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1039450#M6956</guid>
      <dc:creator>Xiang_Li</dc:creator>
      <dc:date>2020-07-30T02:12:18Z</dc:date>
    </item>
    <item>
      <title>Re:  NT3H2111</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1369577#M8991</link>
      <description>&lt;P&gt;Dear,&lt;/P&gt;&lt;P&gt;We wrote session register value 0x41 by i2c write format( s+mema+mask+regdat+stop ), then read it, return value is 0x1...&lt;/P&gt;&lt;P&gt;Has access session register any limited? has nxp sample code for nt3h2111?&amp;nbsp;&lt;/P&gt;&lt;P&gt;thanks your help&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 02:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111/m-p/1369577#M8991</guid>
      <dc:creator>kitconan</dc:creator>
      <dc:date>2021-11-11T02:31:29Z</dc:date>
    </item>
  </channel>
</rss>