<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RFID/NFC tag in NFC</title>
    <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030171#M6871</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jonathaniglesias"&gt;jonathaniglesias&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I think there is a little misunderstanding here. My fault I haven't been enough precise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both protocols will be on the same carrier frequency (HF 13,56MHz). My project is about a card which can be readed by a ISO15693 reader for simple identification and by an NFC reader (like a phone with NFC).&lt;/P&gt;&lt;P&gt;A colleague told me about Desfire tags but didn't know much about detailed functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just would like to know if this tag can choose what to do based only on the protocol used to interact with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Feb 2020 13:30:58 GMT</pubDate>
    <dc:creator>simonschmitt</dc:creator>
    <dc:date>2020-02-13T13:30:58Z</dc:date>
    <item>
      <title>RFID/NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030169#M6869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for a RFID/NFC tag chip able to interract with classic RFID readers (ISO14443) and NFC readers (ISO15693) and who can transmit differents datas depending on the technology used by the reader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've seen the PN7462 is able to interract with these different norms, but it seem that this chip is designed to be inserted in RFID readers as far as I understand it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can this chip be used as a tag or should I take a look at a different NXP family?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jan 2020 14:01:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030169#M6869</guid>
      <dc:creator>simonschmitt</dc:creator>
      <dc:date>2020-01-17T14:01:52Z</dc:date>
    </item>
    <item>
      <title>Re: RFID/NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030170#M6870</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="312614" data-username="simonschmitt" href="https://community.nxp.com/people/simonschmitt"&gt;Simon Schmitt&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great, well in this case we do not have a multi frequency tag,&amp;nbsp; we have tags that can be embedded in a card for example, so the card has a HF and a LF tag inside and depending on the reader frequency is the IC you trigger, but a solution combining both, we do not have, we have a list of manufacturers that have solutions using our ICs that can help you.&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS" title="https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS"&gt;RFID Ecosystem | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;about the PN7462, this is a reader, this reader is a full NFC reader which means that supports&amp;nbsp; the three modes of NFC.&lt;/P&gt;&lt;P&gt;1.- Reader/writer&lt;/P&gt;&lt;P&gt;2.-Card emulation ( ISO 14443)&lt;/P&gt;&lt;P&gt;3.-Peer to peer&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;also this reader has a contact interface for contact cards.&lt;/P&gt;&lt;P&gt;Have a great day !&lt;BR /&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 16:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030170#M6870</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-01-21T16:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: RFID/NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030171#M6871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/jonathaniglesias"&gt;jonathaniglesias&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I think there is a little misunderstanding here. My fault I haven't been enough precise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both protocols will be on the same carrier frequency (HF 13,56MHz). My project is about a card which can be readed by a ISO15693 reader for simple identification and by an NFC reader (like a phone with NFC).&lt;/P&gt;&lt;P&gt;A colleague told me about Desfire tags but didn't know much about detailed functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just would like to know if this tag can choose what to do based only on the protocol used to interact with it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 13:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030171#M6871</guid>
      <dc:creator>simonschmitt</dc:creator>
      <dc:date>2020-02-13T13:30:58Z</dc:date>
    </item>
    <item>
      <title>Re: RFID/NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030172#M6872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Simon,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are doing great, well first I want to be clear in some things, when you use a card in HF ( 13.56MHz) this card can communicate with either an NFC reader and a Vicinity ( ISO 15693) reader, since both protocols support&amp;nbsp; same communication frequency but the issue can come if you want a vicinity reader with an NFC card to be activated at a Vicinity range ( up to 1m). said this, the question is more on the reader side, the card can be activated and communicate with a reader either vicinity or NFC as long as the reader support the command set and provides the minimum energy&amp;nbsp; to activate that card&amp;nbsp; either for interaction or just identification. so if in this case a DESFire is a T4T ( type 4 tag) that supports ISO 14443 commands and also ISO 7816-4. if you implement the activation procedure in the discovery loop of your reader&amp;nbsp; there should not be any issue, like it happens in our PN7462 reader, one of the examples ( Discovery loop)&amp;nbsp; can detect different type of tags&amp;nbsp; from ISO 15693, ISO 14443, P2P, card emulation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Feb 2020 02:19:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030172#M6872</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-02-17T02:19:50Z</dc:date>
    </item>
    <item>
      <title>Re: RFID/NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030173#M6873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jonathan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer.&lt;/P&gt;&lt;P&gt;In my application, vicinity range is not a problem. I will only need 2 to 5 cm range.&lt;/P&gt;&lt;P&gt;You say Desfire tags can communicate with both ISO 14443 reader and ISO 15693 reader but in documentation, I can't see any reference to 15693.&lt;/P&gt;&lt;P&gt;Sorry if the answer of this question is self-evident, I'm quite new to the NFC world.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And when you speak about "discovery loop" of the reader, that mean I can't use an old reader where I can't put my word about it programmation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you again.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2020 16:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030173#M6873</guid>
      <dc:creator>simonschmitt</dc:creator>
      <dc:date>2020-02-21T16:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: RFID/NFC tag</title>
      <link>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030174#M6874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="312614" data-username="simonschmitt" href="https://community.nxp.com/people/simonschmitt" style="color: #3d9ce7; background-color: #ffffff; border: 0px; font-weight: 200; text-decoration: underline; font-size: 1.286rem;"&gt;Simon Schmitt&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great,&amp;nbsp; I said that a vicinity reader is able to communicate with DESFire as long as the firmware inside the reader have the commands to interact with DESFire, this does not mean DESFire support 15693.&lt;/P&gt;&lt;P&gt;I am not sure I am understanding&amp;nbsp; your last question :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;And when you speak about "discovery loop" of the reader, that mean I can't use an old reader where I can't put my word about it programmation?&lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;basically the discovery loop is the polling state where the reader search for different technologies&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96176i05A10826154A0E18/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Feb 2020 14:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RFID-NFC-tag/m-p/1030174#M6874</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-02-25T14:34:32Z</dc:date>
    </item>
  </channel>
</rss>