<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NXP reader library with NTAG I2C Plus</title>
    <link>https://community.nxp.com/t5/NFC/NXP-reader-library-with-NTAG-I2C-Plus/m-p/1025050#M6814</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we want to use the NXP reader library with a NTAG I2C Plus tag (as reader a Pegoda CLRD710 is used). Is there any working example code and/or documenation that shows the usage of the NTAG I2C Plus functionality? The tag shall not be used with NDEF messages, we directly want to read/fastread and write/fastwrite the complete memory, read the signature and the version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Nov 2019 19:50:47 GMT</pubDate>
    <dc:creator>sjardot</dc:creator>
    <dc:date>2019-11-21T19:50:47Z</dc:date>
    <item>
      <title>NXP reader library with NTAG I2C Plus</title>
      <link>https://community.nxp.com/t5/NFC/NXP-reader-library-with-NTAG-I2C-Plus/m-p/1025050#M6814</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we want to use the NXP reader library with a NTAG I2C Plus tag (as reader a Pegoda CLRD710 is used). Is there any working example code and/or documenation that shows the usage of the NTAG I2C Plus functionality? The tag shall not be used with NDEF messages, we directly want to read/fastread and write/fastwrite the complete memory, read the signature and the version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 19:50:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NXP-reader-library-with-NTAG-I2C-Plus/m-p/1025050#M6814</guid>
      <dc:creator>sjardot</dc:creator>
      <dc:date>2019-11-21T19:50:47Z</dc:date>
    </item>
    <item>
      <title>Re: NXP reader library with NTAG I2C Plus</title>
      <link>https://community.nxp.com/t5/NFC/NXP-reader-library-with-NTAG-I2C-Plus/m-p/1025051#M6815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="351647" data-username="sjardot@de.pepperl-fuchs.com" href="https://community.nxp.com/people/sjardot@de.pepperl-fuchs.com"&gt;Stefan Jardot&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great, there is no example for NTAG I2C and pegoda,&amp;nbsp; in the NFC reader library you can find the example for NTAG i2c, this example reads some memory from the NTAG and the write&amp;nbsp; to sector 0 .&lt;/P&gt;&lt;P&gt;the library for pegoda is secured under NDA ( Non Disclosure Agreement) this means that all the information, tools and support. you can use the example available in the NFC reader library in the webpage as reference.&lt;/P&gt;&lt;P&gt;Have a great day !&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Nov 2019 14:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NXP-reader-library-with-NTAG-I2C-Plus/m-p/1025051#M6815</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2019-11-27T14:13:18Z</dc:date>
    </item>
  </channel>
</rss>