<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7120 Notifications. in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7120-Notifications/m-p/1021086#M6797</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am currently working with two PN7120 implemented in development boards ( NFC_click ). I am successfully communicating over I2C using a pic18 with the PN7120 using the NCI.&lt;/P&gt;&lt;P&gt;I configured the PN7120 using RF_DISCOVER_MAP_CMD and RF_DISCOVER_CMD getting the proper Responses with the Status 0x00 (ok). I should now be getting the notification RF_FIELD_INFO_NTF.&lt;/P&gt;&lt;P&gt;I have not recieved any notifications at any point.&lt;/P&gt;&lt;P&gt;As an example the initial CORE_RESET_CMD should result in a response and then a notification, there is no notificiation ever.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone could assist me, or point me in the right direction, I would be grateful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jan 2020 13:41:24 GMT</pubDate>
    <dc:creator>tewexor600</dc:creator>
    <dc:date>2020-01-16T13:41:24Z</dc:date>
    <item>
      <title>PN7120 Notifications.</title>
      <link>https://community.nxp.com/t5/NFC/PN7120-Notifications/m-p/1021086#M6797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I am currently working with two PN7120 implemented in development boards ( NFC_click ). I am successfully communicating over I2C using a pic18 with the PN7120 using the NCI.&lt;/P&gt;&lt;P&gt;I configured the PN7120 using RF_DISCOVER_MAP_CMD and RF_DISCOVER_CMD getting the proper Responses with the Status 0x00 (ok). I should now be getting the notification RF_FIELD_INFO_NTF.&lt;/P&gt;&lt;P&gt;I have not recieved any notifications at any point.&lt;/P&gt;&lt;P&gt;As an example the initial CORE_RESET_CMD should result in a response and then a notification, there is no notificiation ever.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone could assist me, or point me in the right direction, I would be grateful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 13:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7120-Notifications/m-p/1021086#M6797</guid>
      <dc:creator>tewexor600</dc:creator>
      <dc:date>2020-01-16T13:41:24Z</dc:date>
    </item>
    <item>
      <title>Re: PN7120 Notifications.</title>
      <link>https://community.nxp.com/t5/NFC/PN7120-Notifications/m-p/1021087#M6798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Hope you are doing great, have you tried following the exact timings and commands using one of our board with the PN7120, like a FRDM K64 ?&lt;/P&gt;&lt;P&gt;just to confirm anything in the procedure is correct.&lt;/P&gt;&lt;P&gt;Have a great day !&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jan 2020 00:23:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7120-Notifications/m-p/1021087#M6798</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-01-21T00:23:20Z</dc:date>
    </item>
  </channel>
</rss>