<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 Reference code for nfcprogramloader NHS31xx</title>
    <link>https://community.nxp.com/t5/NFC/Reference-code-for-nfcprogramloader-NHS31xx/m-p/1016913#M6757</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on an NHS3152 and in the SDK documentation there is an application "nfcprogramloader" that comes on the demo chips. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This application loads code over NFC into flash on the chip. It looks like it was removed from the SDK "release_mra2_12_1_nhs3152" as the software directory is named "/release_mra2_12_1_nhs3152/sw/nss/app_closed_nfcprogramloader".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The include files and binaries remain, but the C files are gone. I'd like to use it as reference code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this application available anywhere?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is the Android program loader code available as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jan 2020 00:58:18 GMT</pubDate>
    <dc:creator>kevin_fry</dc:creator>
    <dc:date>2020-01-16T00:58:18Z</dc:date>
    <item>
      <title>Reference code for nfcprogramloader NHS31xx</title>
      <link>https://community.nxp.com/t5/NFC/Reference-code-for-nfcprogramloader-NHS31xx/m-p/1016913#M6757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on an NHS3152 and in the SDK documentation there is an application "nfcprogramloader" that comes on the demo chips. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This application loads code over NFC into flash on the chip. It looks like it was removed from the SDK "release_mra2_12_1_nhs3152" as the software directory is named "/release_mra2_12_1_nhs3152/sw/nss/app_closed_nfcprogramloader".&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The include files and binaries remain, but the C files are gone. I'd like to use it as reference code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this application available anywhere?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is the Android program loader code available as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jan 2020 00:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Reference-code-for-nfcprogramloader-NHS31xx/m-p/1016913#M6757</guid>
      <dc:creator>kevin_fry</dc:creator>
      <dc:date>2020-01-16T00:58:18Z</dc:date>
    </item>
    <item>
      <title>Re: Reference code for nfcprogramloader NHS31xx</title>
      <link>https://community.nxp.com/t5/NFC/Reference-code-for-nfcprogramloader-NHS31xx/m-p/1016914#M6758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The source code for the&amp;nbsp;NFC one-time Program Loader has never been released.&amp;nbsp;The single header file that is included describes the different NDEF MIME record payloads that can be&amp;nbsp;exchanged with a tag reader. An APP developer can use this to create a fully functioning APP himself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At this moment there are no plans to release the firmware source code, nor the Android APP source code. If you have a business case that&amp;nbsp;requires this, please contact a&amp;nbsp;local NXP sales representative. Note that we have released the source code of both the firmware and the phone APPs of the temperature logger demo and other demo's.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;BR /&gt;Dries.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jan 2020 21:01:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Reference-code-for-nfcprogramloader-NHS31xx/m-p/1016914#M6758</guid>
      <dc:creator>driesmoors</dc:creator>
      <dc:date>2020-01-19T21:01:24Z</dc:date>
    </item>
  </channel>
</rss>