<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 NFC Tag Emulation &amp; iOS + Android</title>
    <link>https://community.nxp.com/t5/NFC/NFC-Tag-Emulation-iOS-Android/m-p/1014339#M6711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have an application whereby I need a NFC Controller, a user scans the&amp;nbsp;device and is directed to a web-site.&lt;/P&gt;&lt;P&gt;The URI must be programmable and prefer a controller over a frontend.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can an Iphone (7 onwards) or Android phone auto scan/read a&amp;nbsp;PN7462 and then be directed to a web-site as per the information in NDEF URI?&lt;/P&gt;&lt;P&gt;And this website could be varied based on some info coming through SPI/I2C or USB etc?&lt;/P&gt;&lt;P&gt;Does there need to be a specific App developed on the phone or will a pop-up be presented where the user can accept and then be directed to the web-site?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Thanks for your support!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Mar 2020 00:56:01 GMT</pubDate>
    <dc:creator>sujit1</dc:creator>
    <dc:date>2020-03-11T00:56:01Z</dc:date>
    <item>
      <title>NFC Tag Emulation &amp; iOS + Android</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Tag-Emulation-iOS-Android/m-p/1014339#M6711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have an application whereby I need a NFC Controller, a user scans the&amp;nbsp;device and is directed to a web-site.&lt;/P&gt;&lt;P&gt;The URI must be programmable and prefer a controller over a frontend.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can an Iphone (7 onwards) or Android phone auto scan/read a&amp;nbsp;PN7462 and then be directed to a web-site as per the information in NDEF URI?&lt;/P&gt;&lt;P&gt;And this website could be varied based on some info coming through SPI/I2C or USB etc?&lt;/P&gt;&lt;P&gt;Does there need to be a specific App developed on the phone or will a pop-up be presented where the user can accept and then be directed to the web-site?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Thanks for your support!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2020 00:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Tag-Emulation-iOS-Android/m-p/1014339#M6711</guid>
      <dc:creator>sujit1</dc:creator>
      <dc:date>2020-03-11T00:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Tag Emulation &amp; iOS + Android</title>
      <link>https://community.nxp.com/t5/NFC/NFC-Tag-Emulation-iOS-Android/m-p/1014340#M6712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are doing well. The PN7462 is Full NFC Forum and EMVCo 2.6 compliant&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Read/Write, Card Emulation &amp;amp; Peer-to-Peer Modes.&lt;/LI&gt;&lt;LI&gt;Full MIFARE family support and ISO/IEC 14443 Type A&amp;amp;B licensed.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IOS phones can interact with a reader in card emulation mode, (so the PN7462 is a good choice). So you will be able to use your IOS or Android phone with the reader in card emulation mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PN7462 has four different interfaces for host connection: USB, HSUART, I2C and SPI.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is no needed a special App. If the NDEF message is correct, the phone will automatically directed to the web site.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also please check our NTAG 424 family this tags have a feature called SDM&amp;nbsp; (Secure Dynamic Messaging) this can create an dynamic URL NDEF, please check if this can be solved with that family of tags as well.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 13:44:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NFC-Tag-Emulation-iOS-Android/m-p/1014340#M6712</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2020-03-13T13:44:16Z</dc:date>
    </item>
  </channel>
</rss>