<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックUSB Errors on ESD test</title>
    <link>https://community.nxp.com/t5/NFC/USB-Errors-on-ESD-test/m-p/1009504#M6640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PN7462 for both smart card and NFC card reader.&lt;/P&gt;&lt;P&gt;I am suffering a problem with the ESD test.&lt;/P&gt;&lt;P&gt;USB communication will get lost in the ESD test but the device didn't aware of the situation.&lt;/P&gt;&lt;P&gt;The CPU is alive therefore watchdog is useless.&lt;/P&gt;&lt;P&gt;I am using like short D+/D- to simulate the ESD interference condition.&lt;/P&gt;&lt;P&gt;I discovered nothing abnormal from USB registers even the D+/D-&amp;nbsp; is shorted&lt;/P&gt;&lt;P&gt;The attached is the error counts from USB ISR.&lt;/P&gt;&lt;P&gt;To compare the snapshots, before and after D+/D- shorts, I got some questions:&lt;/P&gt;&lt;P&gt;#1. I got some NAK errors (isr_err[9]) even I did NOT enable the IntOnNak_AI/&lt;SPAN&gt;IntOnNak_AO/IntOnNak_CI/IntOnNak_CO bits of command/status register, before D+/D- get shorted. Where are they from and how?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#2. There is a sent stall error (isr_err[10]). I guess it is from the enumeration process but why?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I did NOT find any abnormal&amp;nbsp;during&amp;nbsp;enumeration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#3. After D+/D- get shorted, I tried several times and 2 samples attached.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;One is reported truncated EOP (isr_err[8]) and one is reported bit stuff error (isr_err[13]). They are not always reported.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#4 What is the best way to detect USB interface errors. Original I&amp;nbsp; think it can be detected by SOF and NAK of interrupt endpoint. Both of them could be beacons between the USB host and the device. However, I can get SOF and NAK ISRs when the D+/D- get shorted, but I think the communication between the USB host and the device actually gets lost since card insertion even is bot work anymore.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are there any registers that need to be set to properly detect SOF/NAK behavior correctly?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jack&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 22 Dec 2019 17:27:31 GMT</pubDate>
    <dc:creator>jackchan</dc:creator>
    <dc:date>2019-12-22T17:27:31Z</dc:date>
    <item>
      <title>USB Errors on ESD test</title>
      <link>https://community.nxp.com/t5/NFC/USB-Errors-on-ESD-test/m-p/1009504#M6640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PN7462 for both smart card and NFC card reader.&lt;/P&gt;&lt;P&gt;I am suffering a problem with the ESD test.&lt;/P&gt;&lt;P&gt;USB communication will get lost in the ESD test but the device didn't aware of the situation.&lt;/P&gt;&lt;P&gt;The CPU is alive therefore watchdog is useless.&lt;/P&gt;&lt;P&gt;I am using like short D+/D- to simulate the ESD interference condition.&lt;/P&gt;&lt;P&gt;I discovered nothing abnormal from USB registers even the D+/D-&amp;nbsp; is shorted&lt;/P&gt;&lt;P&gt;The attached is the error counts from USB ISR.&lt;/P&gt;&lt;P&gt;To compare the snapshots, before and after D+/D- shorts, I got some questions:&lt;/P&gt;&lt;P&gt;#1. I got some NAK errors (isr_err[9]) even I did NOT enable the IntOnNak_AI/&lt;SPAN&gt;IntOnNak_AO/IntOnNak_CI/IntOnNak_CO bits of command/status register, before D+/D- get shorted. Where are they from and how?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#2. There is a sent stall error (isr_err[10]). I guess it is from the enumeration process but why?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I did NOT find any abnormal&amp;nbsp;during&amp;nbsp;enumeration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#3. After D+/D- get shorted, I tried several times and 2 samples attached.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;One is reported truncated EOP (isr_err[8]) and one is reported bit stuff error (isr_err[13]). They are not always reported.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;#4 What is the best way to detect USB interface errors. Original I&amp;nbsp; think it can be detected by SOF and NAK of interrupt endpoint. Both of them could be beacons between the USB host and the device. However, I can get SOF and NAK ISRs when the D+/D- get shorted, but I think the communication between the USB host and the device actually gets lost since card insertion even is bot work anymore.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Are there any registers that need to be set to properly detect SOF/NAK behavior correctly?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jack&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 22 Dec 2019 17:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/USB-Errors-on-ESD-test/m-p/1009504#M6640</guid>
      <dc:creator>jackchan</dc:creator>
      <dc:date>2019-12-22T17:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: USB Errors on ESD test</title>
      <link>https://community.nxp.com/t5/NFC/USB-Errors-on-ESD-test/m-p/1009505#M6641</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PNEV7462 board is ok with USB certificate, please kindly refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99540i79AACF032D58FFD4/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I think it should be a hardware design issue, please refer to the ref board schematics (UM10883 )and check if there is&amp;nbsp; any difference .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BTW, what is the ESD voltage level performed on PN7462?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Dec 2019 09:51:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/USB-Errors-on-ESD-test/m-p/1009505#M6641</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-12-24T09:51:47Z</dc:date>
    </item>
  </channel>
</rss>