<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Type B,F and V detection using example  NFCrdlibEX4_Mifare classic with CLRC663  in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Type-B-F-and-V-detection-using-example-NFCrdlibEX4-Mifare/m-p/1001521#M6549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm using CLRC663&amp;nbsp; with STM32 for my project.I want to detect all types of tags i.e Type A,B,F and V.The example i followed is NfcrdlibEx4_MifareClassic.I have enabled all the necessary macros for all types of tag.But i dint get type B,F and V other than Type A.I have changed only the driver file so as to work with stm32.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also I tried the same&amp;nbsp;&lt;SPAN&gt;NfcrdlibEx4_MifareClassic example&lt;/SPAN&gt; in the&amp;nbsp;&lt;SPAN&gt;CLEV6630B&lt;/SPAN&gt;&amp;nbsp;v2.0 development board and i got it working for all tag types.But in my project ,&lt;SPAN&gt;it dint work except type A. The difference between my project and development board is only the MCU but the reader IC is same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Whenever type B,F and V tags&amp;nbsp; are shown in the field,CLRC always return "No Tech Detected". It only detects type A tag.&lt;/P&gt;&lt;P&gt;when i debugged the firmware, i found out that only "TX-IRQ" sets for type B,F&amp;amp;V and "RX-IRQ" does not set. Whereas for Type A both "TX-IRQ" and "RX-IRq" set.&lt;/P&gt;&lt;P&gt;Could&amp;nbsp;anyone please help me out in this .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Dec 2019 07:39:36 GMT</pubDate>
    <dc:creator>shobana1</dc:creator>
    <dc:date>2019-12-19T07:39:36Z</dc:date>
    <item>
      <title>Type B,F and V detection using example  NFCrdlibEX4_Mifare classic with CLRC663</title>
      <link>https://community.nxp.com/t5/NFC/Type-B-F-and-V-detection-using-example-NFCrdlibEX4-Mifare/m-p/1001521#M6549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;I'm using CLRC663&amp;nbsp; with STM32 for my project.I want to detect all types of tags i.e Type A,B,F and V.The example i followed is NfcrdlibEx4_MifareClassic.I have enabled all the necessary macros for all types of tag.But i dint get type B,F and V other than Type A.I have changed only the driver file so as to work with stm32.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also I tried the same&amp;nbsp;&lt;SPAN&gt;NfcrdlibEx4_MifareClassic example&lt;/SPAN&gt; in the&amp;nbsp;&lt;SPAN&gt;CLEV6630B&lt;/SPAN&gt;&amp;nbsp;v2.0 development board and i got it working for all tag types.But in my project ,&lt;SPAN&gt;it dint work except type A. The difference between my project and development board is only the MCU but the reader IC is same.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Whenever type B,F and V tags&amp;nbsp; are shown in the field,CLRC always return "No Tech Detected". It only detects type A tag.&lt;/P&gt;&lt;P&gt;when i debugged the firmware, i found out that only "TX-IRQ" sets for type B,F&amp;amp;V and "RX-IRQ" does not set. Whereas for Type A both "TX-IRQ" and "RX-IRq" set.&lt;/P&gt;&lt;P&gt;Could&amp;nbsp;anyone please help me out in this .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 07:39:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Type-B-F-and-V-detection-using-example-NFCrdlibEX4-Mifare/m-p/1001521#M6549</guid>
      <dc:creator>shobana1</dc:creator>
      <dc:date>2019-12-19T07:39:36Z</dc:date>
    </item>
    <item>
      <title>Re: Type B,F and V detection using example  NFCrdlibEX4_Mifare classic with CLRC663</title>
      <link>https://community.nxp.com/t5/NFC/Type-B-F-and-V-detection-using-example-NFCrdlibEX4-Mifare/m-p/1001522#M6550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Shobana,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NfcrdlibEx1_BasicDiscoveryLoop demo supports Type A,B,F and V tag detection, you may start your application based on that. The &lt;SPAN&gt;NfcrdlibEx4_MifareClassic example&lt;/SPAN&gt; just supports type A tag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Dec 2019 08:45:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Type-B-F-and-V-detection-using-example-NFCrdlibEX4-Mifare/m-p/1001522#M6550</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-12-25T08:45:39Z</dc:date>
    </item>
  </channel>
</rss>