<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックDoes Ucode8 support self-serialization?</title>
    <link>https://community.nxp.com/t5/NFC/Does-Ucode8-support-self-serialization/m-p/994372#M6452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello - We have a customer which has been using Ucode7 RFID tags for some time in a self-serialization workflow. However, when they tried to use Ucode8 tags in the same capacity, the EPCs always seems to encode as a "0" (see attached). Can anyone here confirm or deny if self-serialization (may "auto-serialization" is the correct term) is supported with the Ucode8 tags? I see that the memory mapping is a bit different on the chips but it looks like there should still be enough room for our 96-bit EPC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The customer is using Impinj ItemEncode 2.4.3.240, but when I asked Impinj, they were under the impression that the tags themselves performed the serialization, not the encoders.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance all for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Dec 2019 14:22:20 GMT</pubDate>
    <dc:creator>davide1</dc:creator>
    <dc:date>2019-12-02T14:22:20Z</dc:date>
    <item>
      <title>Does Ucode8 support self-serialization?</title>
      <link>https://community.nxp.com/t5/NFC/Does-Ucode8-support-self-serialization/m-p/994372#M6452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello - We have a customer which has been using Ucode7 RFID tags for some time in a self-serialization workflow. However, when they tried to use Ucode8 tags in the same capacity, the EPCs always seems to encode as a "0" (see attached). Can anyone here confirm or deny if self-serialization (may "auto-serialization" is the correct term) is supported with the Ucode8 tags? I see that the memory mapping is a bit different on the chips but it looks like there should still be enough room for our 96-bit EPC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The customer is using Impinj ItemEncode 2.4.3.240, but when I asked Impinj, they were under the impression that the tags themselves performed the serialization, not the encoders.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance all for your help!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2019 14:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Does-Ucode8-support-self-serialization/m-p/994372#M6452</guid>
      <dc:creator>davide1</dc:creator>
      <dc:date>2019-12-02T14:22:20Z</dc:date>
    </item>
    <item>
      <title>Re: Does Ucode8 support self-serialization?</title>
      <link>https://community.nxp.com/t5/NFC/Does-Ucode8-support-self-serialization/m-p/994373#M6453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear&amp;nbsp;&lt;A _jive_internal="true" data-userid="352322" data-username="davide@thesolutionsgroup.com" href="https://community.nxp.com/people/davide@thesolutionsgroup.com"&gt;David Endahl&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Hope you are doing great,&amp;nbsp;pre-serialization means that&amp;nbsp; NXP pre program the TID and mirror that into the EPC memory this is usually how we deliver products, we are not 100% sure what you mean by "auto-serialization", the only main difference that comes right to my minds is the parallel encoding.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jonathan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2020 14:16:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Does-Ucode8-support-self-serialization/m-p/994373#M6453</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-01-09T14:16:16Z</dc:date>
    </item>
  </channel>
</rss>