<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: NT3H2111 Running With 5V</title>
    <link>https://community.nxp.com/t5/NFC/NT3H2111-Running-With-5V/m-p/993274#M6439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;There is the same question with you in case. Please refer to the case and you will receive the feedback via email. Have a nice day.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Dec 2019 07:30:35 GMT</pubDate>
    <dc:creator>fangfang</dc:creator>
    <dc:date>2019-12-18T07:30:35Z</dc:date>
    <item>
      <title>NT3H2111 Running With 5V</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-Running-With-5V/m-p/993273#M6438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a design that needs to run&amp;nbsp;with 5V Vcc. The microcontroller that talks to the&amp;nbsp;NT3H2111 chip runs&amp;nbsp;with 5V. According to the&amp;nbsp;NT3H2111 datasheet, this chip work between 1.67V and 3.6V. Do you have a chip like the&amp;nbsp;NT3H2111 that works with 5V? We don't want to use level converters or anything like that.&amp;nbsp;We need a simple inexpensive solution. Do you have any suggestions or ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 21:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-Running-With-5V/m-p/993273#M6438</guid>
      <dc:creator>robertosocorreg</dc:creator>
      <dc:date>2019-12-17T21:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: NT3H2111 Running With 5V</title>
      <link>https://community.nxp.com/t5/NFC/NT3H2111-Running-With-5V/m-p/993274#M6439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;There is the same question with you in case. Please refer to the case and you will receive the feedback via email. Have a nice day.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2019 07:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/NT3H2111-Running-With-5V/m-p/993274#M6439</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2019-12-18T07:30:35Z</dc:date>
    </item>
  </channel>
</rss>