<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7462 ROM3 functions definition</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-ROM3-functions-definition/m-p/989375#M6395</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Where can I find a complete definition for the HAL functions mapped in ROM3 ?&lt;/P&gt;&lt;P&gt;I have the NXP NFC reader library including the following HTML file&lt;/P&gt;&lt;P&gt;PN7462AU-FW_v05.22.01_Full\ApiDocumentation\PN7462AU\PN7462AU-FW-apiguide.html&lt;/P&gt;&lt;P&gt;and also UM10913 document but whatever it doesn't give the addresses (I got them from PN7462AU\phCommon\inc\PN7462AU_ROM3.h file but it is not a specification) of the functions neither the parameters specification.&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Julie Ronday&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jan 2020 13:14:17 GMT</pubDate>
    <dc:creator>julieronday</dc:creator>
    <dc:date>2020-01-09T13:14:17Z</dc:date>
    <item>
      <title>PN7462 ROM3 functions definition</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-ROM3-functions-definition/m-p/989375#M6395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Where can I find a complete definition for the HAL functions mapped in ROM3 ?&lt;/P&gt;&lt;P&gt;I have the NXP NFC reader library including the following HTML file&lt;/P&gt;&lt;P&gt;PN7462AU-FW_v05.22.01_Full\ApiDocumentation\PN7462AU\PN7462AU-FW-apiguide.html&lt;/P&gt;&lt;P&gt;and also UM10913 document but whatever it doesn't give the addresses (I got them from PN7462AU\phCommon\inc\PN7462AU_ROM3.h file but it is not a specification) of the functions neither the parameters specification.&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Julie Ronday&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jan 2020 13:14:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-ROM3-functions-definition/m-p/989375#M6395</guid>
      <dc:creator>julieronday</dc:creator>
      <dc:date>2020-01-09T13:14:17Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 ROM3 functions definition</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-ROM3-functions-definition/m-p/989376#M6396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;They are not functions but defined addresses which are used in other files, e.g. PH_HAL_GPIO_CONFIGOUTPUT_ADDR (0x00007fd9) is used in file&amp;nbsp;phhalGpio.h below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"PN7462AU_ROM3.h"&lt;/SPAN&gt;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"ph_Status.h"&lt;/SPAN&gt;&lt;/SPAN&gt;

&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;

&lt;SPAN class="property macro token"&gt;#define phhalPcr_ConfigOutput(dwGpioNumber, dwEnableAsOuput, dwSlewRate) \
((phhalPcr_ConfigOutput_t *) \
PH_HAL_GPIO_CONFIGOUTPUT_ADDR)\
(dwGpioNumber, dwEnableAsOuput, dwSlewRate) ‍‍‍‍‍‍‍‍‍‍‍‍‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jan 2020 22:40:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-ROM3-functions-definition/m-p/989376#M6396</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2020-01-20T22:40:44Z</dc:date>
    </item>
  </channel>
</rss>