<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PN7462 Card ID read APDU in NFC</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987884#M6376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Utsavi B.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looks like you prefer to mostly focus on the application layer, so maybe a ready USB NFC reader is what you are looking for, but we are just IC supplier so we only have NFC reader solution such as PN7462AU, which has a CCID demo might be close to your requirement, but you still have to build your own application based on that.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96448i8C994AA72FD181D5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to UM10915 for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Dec 2019 06:58:19 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2019-12-11T06:58:19Z</dc:date>
    <item>
      <title>PN7462 Card ID read APDU</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987881#M6373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with PN 7462 reader. I go through application notes of UM10915.pdf.&amp;nbsp; As compare to PN532, few commands are available for PN7462.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here, command that read the tag (ex, commands to read tag for pn532 is InList Passive Target to read Tags from RF field ) .&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But no such command&amp;nbsp; is provided for PN7462.Is ATR contains TAG CID? If not then Is any of doc for this availabale?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my application, I want to read Mifare Ultralight,Classic and DESFire cards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using which command, I can send all DESFire commands. For example in PN532 using InDataExchange command, in [data] , DESFire native command can be written.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And I want to use DESFire commands like,Auth&amp;nbsp; Card ,Change Key, Create Application, Select application, Select tag, read, write, createstd file etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One more thing what is use of Value file in DESFire..?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Utsavi B&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2019 09:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987881#M6373</guid>
      <dc:creator>utsavikalpesh</dc:creator>
      <dc:date>2019-11-29T09:10:07Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Card ID read APDU</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987882#M6374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Utsavi B,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually PN7462 is a different product from PN532, so you can not use the same way of PN532 with PN7462, regarding which you may understand it as a MCU + NFC frontend, so you have to program custom application and download it into PN7462, you know, this provides more flexibility but makes things more complicated , while we provide NFC reader library for this device, with demos as well, you may find Mifare Classic and Desfire demo there. Please kindly refer to &lt;A class="link-titled" href="https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY" title="https://www.nxp.com/design/designs/nfc-reader-library-software-support-for-nfc-frontend-solutions:NFC-READER-LIBRARY"&gt;NFC Reader Library | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 03:18:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987882#M6374</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-12-09T03:18:20Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Card ID read APDU</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987883#M6375</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Isn't it possible that using APDU provided by PN7462 user guide, I send command to reader and get response from reader?? Irrespective of NFC reader library. NFC Reader lib seems complicate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want something like NFC which I do not need to modify, which will perform Tag and Reader communication. And another application, which will respond my commands and get me a Tag.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using above concept I will prepare command for PN7462 instead of PN532, without taking care of NFC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Utsavi B.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Dec 2019 05:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987883#M6375</guid>
      <dc:creator>utsavikalpesh</dc:creator>
      <dc:date>2019-12-09T05:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Card ID read APDU</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987884#M6376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Utsavi B.,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looks like you prefer to mostly focus on the application layer, so maybe a ready USB NFC reader is what you are looking for, but we are just IC supplier so we only have NFC reader solution such as PN7462AU, which has a CCID demo might be close to your requirement, but you still have to build your own application based on that.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96448i8C994AA72FD181D5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to UM10915 for more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Dec 2019 06:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/987884#M6376</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-12-11T06:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Card ID read APDU</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/1189725#M7926</link>
      <description>&lt;P&gt;Hi, I'm working on the NXP PN7462, I wanted to ask you if it supports all standard APDU commands (ISO7816-4) or just a part. In particular, I would need the following:&lt;BR /&gt;// APDU commands&lt;BR /&gt;enum eApduCmds {&lt;BR /&gt;CMD_CREATE_FILE = 0xE0,&lt;BR /&gt;CMD_CHANGE = 0x24,&lt;BR /&gt;CMD_DELETE_FILE = 0xE4,&lt;BR /&gt;CMD_GET_RESPONSE = 0xC0,&lt;BR /&gt;CMD_GET_STATUS = 0x3C,&lt;BR /&gt;CMD_READ_BINARY = 0xB0,&lt;BR /&gt;CMD_SELECT = 0xA4,&lt;BR /&gt;CMD_UNBLOCK = 0x22,&lt;BR /&gt;CMD_UPDATE_BINARY = 0xD6,&lt;BR /&gt;CMD_VERIFY = 0x20&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Gianluca&lt;/P&gt;</description>
      <pubDate>Thu, 26 Nov 2020 12:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Card-ID-read-APDU/m-p/1189725#M7926</guid>
      <dc:creator>gianlucasofia</dc:creator>
      <dc:date>2020-11-26T12:21:00Z</dc:date>
    </item>
  </channel>
</rss>