<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RC522 compatibility with EM4423 in NFC</title>
    <link>https://community.nxp.com/t5/NFC/RC522-compatibility-with-EM4423/m-p/971862#M6211</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know if the RC522 module can read the EPC Memory bank&amp;nbsp; (NFC blocks 69 to 73)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the specs of the chip these blocks are readable from the NFC but write protected which is fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Em4423 is ISO/IEC 14443 NFC Type 2 the datasheet is attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Sep 2019 16:34:13 GMT</pubDate>
    <dc:creator>mazevedo</dc:creator>
    <dc:date>2019-09-10T16:34:13Z</dc:date>
    <item>
      <title>RC522 compatibility with EM4423</title>
      <link>https://community.nxp.com/t5/NFC/RC522-compatibility-with-EM4423/m-p/971862#M6211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know if the RC522 module can read the EPC Memory bank&amp;nbsp; (NFC blocks 69 to 73)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the specs of the chip these blocks are readable from the NFC but write protected which is fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Em4423 is ISO/IEC 14443 NFC Type 2 the datasheet is attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Sep 2019 16:34:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-compatibility-with-EM4423/m-p/971862#M6211</guid>
      <dc:creator>mazevedo</dc:creator>
      <dc:date>2019-09-10T16:34:13Z</dc:date>
    </item>
    <item>
      <title>Re: RC522 compatibility with EM4423</title>
      <link>https://community.nxp.com/t5/NFC/RC522-compatibility-with-EM4423/m-p/971863#M6212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to &lt;A href="https://www.nxp.com/docs/en/data-sheet/MFRC522.pdf"&gt;datasheet&lt;/A&gt; this product does not support ISO/IEC 18000-63, but ISO/IEC 14443 for which it will not be able to handle EPC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Sep 2019 17:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-compatibility-with-EM4423/m-p/971863#M6212</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-09-13T17:03:53Z</dc:date>
    </item>
  </channel>
</rss>