<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: Android HCE with PN7150 as reader</title>
    <link>https://community.nxp.com/t5/NFC/Android-HCE-with-PN7150-as-reader/m-p/969743#M6199</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that the Android device supports the full features of a real card and that it is not only demodulating the carrier as a e.g. type A tag and responding to anti-collision. The PN7150 will have to be treated as a normal Reader/Writer, it is rather necessary to check e.g. the card commands and timings for a proper integration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Jul 2019 22:18:30 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2019-07-25T22:18:30Z</dc:date>
    <item>
      <title>Android HCE with PN7150 as reader</title>
      <link>https://community.nxp.com/t5/NFC/Android-HCE-with-PN7150-as-reader/m-p/969742#M6198</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Trying to use the PN7150 as a reader that works with Android HCE (host card emulation). Android HCE with Android as a reader works fine with the standard APDU commands, but I don't see any documentation with regards to this for the PN7150.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any resources or examples on the PN7150 that is helpful for this kind of project? Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 13:00:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Android-HCE-with-PN7150-as-reader/m-p/969742#M6198</guid>
      <dc:creator>erik_su</dc:creator>
      <dc:date>2019-07-25T13:00:52Z</dc:date>
    </item>
    <item>
      <title>Re: Android HCE with PN7150 as reader</title>
      <link>https://community.nxp.com/t5/NFC/Android-HCE-with-PN7150-as-reader/m-p/969743#M6199</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure that the Android device supports the full features of a real card and that it is not only demodulating the carrier as a e.g. type A tag and responding to anti-collision. The PN7150 will have to be treated as a normal Reader/Writer, it is rather necessary to check e.g. the card commands and timings for a proper integration.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jul 2019 22:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Android-HCE-with-PN7150-as-reader/m-p/969743#M6199</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-07-25T22:18:30Z</dc:date>
    </item>
  </channel>
</rss>