<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Complex Logic for Discovery Loop in NFC</title>
    <link>https://community.nxp.com/t5/NFC/Complex-Logic-for-Discovery-Loop/m-p/968242#M6177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I need to implement a loop where a Layer 4 Type A card with a specific application is selected and any other type of card is ignored. Even if multiple card types or multiple Layer 4 Type A cards are on the reader the reader must select with the Layer 4 Type A with the correct application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i achive this with the discovery loop.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Jun 2019 13:19:38 GMT</pubDate>
    <dc:creator>aceviker</dc:creator>
    <dc:date>2019-06-10T13:19:38Z</dc:date>
    <item>
      <title>Complex Logic for Discovery Loop</title>
      <link>https://community.nxp.com/t5/NFC/Complex-Logic-for-Discovery-Loop/m-p/968242#M6177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I need to implement a loop where a Layer 4 Type A card with a specific application is selected and any other type of card is ignored. Even if multiple card types or multiple Layer 4 Type A cards are on the reader the reader must select with the Layer 4 Type A with the correct application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i achive this with the discovery loop.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jun 2019 13:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Complex-Logic-for-Discovery-Loop/m-p/968242#M6177</guid>
      <dc:creator>aceviker</dc:creator>
      <dc:date>2019-06-10T13:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: Complex Logic for Discovery Loop</title>
      <link>https://community.nxp.com/t5/NFC/Complex-Logic-for-Discovery-Loop/m-p/968243#M6178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The discovery loop will only poll for types, the switching to Layer 4 and selection of the correct Tag with specific information shall be carried out on the application side.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 16:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/Complex-Logic-for-Discovery-Loop/m-p/968243#M6178</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-06-11T16:31:05Z</dc:date>
    </item>
  </channel>
</rss>