<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックPN7462 Stack Issue</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-Stack-Issue/m-p/963667#M6130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why local variables in a SPIM R/W function (&amp;nbsp;access to /&amp;nbsp;from a NOR flash ) fails read / write to SPIM bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, Accessing to/from NOR flash using global variables with the same SPIM R/W function results with no error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the problem? By the way, the project uses no RTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jun 2019 18:24:50 GMT</pubDate>
    <dc:creator>mukadder</dc:creator>
    <dc:date>2019-06-24T18:24:50Z</dc:date>
    <item>
      <title>PN7462 Stack Issue</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Stack-Issue/m-p/963667#M6130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why local variables in a SPIM R/W function (&amp;nbsp;access to /&amp;nbsp;from a NOR flash ) fails read / write to SPIM bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, Accessing to/from NOR flash using global variables with the same SPIM R/W function results with no error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What can be the problem? By the way, the project uses no RTOS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 18:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Stack-Issue/m-p/963667#M6130</guid>
      <dc:creator>mukadder</dc:creator>
      <dc:date>2019-06-24T18:24:50Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 Stack Issue</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-Stack-Issue/m-p/963668#M6131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looks like a software issue, is the optimization too high? Please try a lower level and check if it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 07:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-Stack-Issue/m-p/963668#M6131</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-06-26T07:41:09Z</dc:date>
    </item>
  </channel>
</rss>