<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFCのトピックRe: RC522. Communication with an active PICC</title>
    <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960103#M6098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know if that frame pattern that in-text&amp;nbsp;I quote above is something standardized? Something described in the ISO 14443-4 probably? I couldn't find more information about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Oct 2019 10:31:04 GMT</pubDate>
    <dc:creator>ccanon</dc:creator>
    <dc:date>2019-10-15T10:31:04Z</dc:date>
    <item>
      <title>RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960098#M6093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi to all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to work with the RC522 reader and an active PICC (AS3953 from AMS). So far I have been able to set both at ISO 14443A Level-4 Protocol Mode. So now I should be able to communicate in both ways. I'm able to send data from PCD--&amp;gt;PICC, but no the other way. PCD buffer remains empty after sending data. I'm afraid that the problem could be the prologue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have read that&amp;nbsp;The ISO 144443A Logic recognizes the command by observing the first received byte. The next&amp;nbsp;picture is a screenshot of the PICC datasheet, where I can see the meaning of the first byte of the ISO block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/81105i598CF8DDE69FCC8E/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is, is there any table, similar to the previous one, but with the values of the first byte of the ISO 14443-4 &lt;STRONG&gt;PICC&lt;/STRONG&gt; block&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Carlos Canón&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 15:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960098#M6093</guid>
      <dc:creator>ccanon</dc:creator>
      <dc:date>2019-10-08T15:42:55Z</dc:date>
    </item>
    <item>
      <title>Re: RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960099#M6094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you try your RC522 board with other tag/card? for example, a mifare card. Did it fail as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 06:51:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960099#M6094</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-10-11T06:51:06Z</dc:date>
    </item>
    <item>
      <title>Re: RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960100#M6095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, I did try with a Mifare classic&amp;nbsp; PICC and works well (it reads the eeprom).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But for my project, I need to be able to transmit data from the PICC to the PCD, that's why I'm using the AMS PICC, because I can control the PICC via SPI and is compliant with ISO 14443-4, which as I understand it should let me send data from PICC -&amp;gt; PCD. Am I wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 07:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960100#M6095</guid>
      <dc:creator>ccanon</dc:creator>
      <dc:date>2019-10-11T07:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960101#M6096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally can get some data transmitted from the PICC to the PCD. I wrongly set up for the receiving data.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I'm using the Receive command to&amp;nbsp;activates the receiver circuits.&amp;nbsp;I'm having problems to send a data chain. For example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;- If I try to send 3 bytes PICC --&amp;gt; PCD : [0x11] [0x12] [0x13],&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;- In the PCD I get [0x11] [0x00]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think this may be due to the frame pattern, but I can't find more information about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/91332iB258877E39EFC06B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know where can I find more details about how to indicate the end of frame pattern or the length byte?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos Canon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 15:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960101#M6096</guid>
      <dc:creator>ccanon</dc:creator>
      <dc:date>2019-10-11T15:38:11Z</dc:date>
    </item>
    <item>
      <title>Re: RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960102#M6097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since your RC522 board can work with a Mifare classic picc, there should be no problem with its hardware and software.Maybe you should contact AMS for further support on AS3953.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 07:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960102#M6097</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-10-15T07:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960103#M6098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kan,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you know if that frame pattern that in-text&amp;nbsp;I quote above is something standardized? Something described in the ISO 14443-4 probably? I couldn't find more information about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 10:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960103#M6098</guid>
      <dc:creator>ccanon</dc:creator>
      <dc:date>2019-10-15T10:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: RC522. Communication with an active PICC</title>
      <link>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960104#M6099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you can trust the data sheet though I am not familiar with the PICC you choose. The data in that table should be complied with ISO14443-4 spec, and I checked the pattern for RATS and DESELECT which should be correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Oct 2019 08:49:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/RC522-Communication-with-an-active-PICC/m-p/960104#M6099</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-10-17T08:49:01Z</dc:date>
    </item>
  </channel>
</rss>