<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MFRC522 - TX1 and TX2 Impedance Matching in NFC</title>
    <link>https://community.nxp.com/t5/NFC/MFRC522-TX1-and-TX2-Impedance-Matching/m-p/952203#M5979</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a RFID Module using MFRC522 chip. So while designing the layout of the board, I wanted to confirm the impedance matching to be performed on TX1 and Tx2 lines . I want my Rmatch to be 50 Ohms. Then do I need both TX1 and Tx2 traces to be 50 Ohms single endedly or should the differential impedance between them be 50 ? I think it is differential but still I would like it confirmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Soumya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jul 2019 10:50:16 GMT</pubDate>
    <dc:creator>spanda</dc:creator>
    <dc:date>2019-07-08T10:50:16Z</dc:date>
    <item>
      <title>MFRC522 - TX1 and TX2 Impedance Matching</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-TX1-and-TX2-Impedance-Matching/m-p/952203#M5979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am designing a RFID Module using MFRC522 chip. So while designing the layout of the board, I wanted to confirm the impedance matching to be performed on TX1 and Tx2 lines . I want my Rmatch to be 50 Ohms. Then do I need both TX1 and Tx2 traces to be 50 Ohms single endedly or should the differential impedance between them be 50 ? I think it is differential but still I would like it confirmed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Soumya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jul 2019 10:50:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-TX1-and-TX2-Impedance-Matching/m-p/952203#M5979</guid>
      <dc:creator>spanda</dc:creator>
      <dc:date>2019-07-08T10:50:16Z</dc:date>
    </item>
    <item>
      <title>Re: MFRC522 - TX1 and TX2 Impedance Matching</title>
      <link>https://community.nxp.com/t5/NFC/MFRC522-TX1-and-TX2-Impedance-Matching/m-p/952204#M5980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As mentioned in the case, the matching has to be done for the antenna values, and&amp;nbsp; the distances between components in the matching circuit shall be as short as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 21:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/MFRC522-TX1-and-TX2-Impedance-Matching/m-p/952204#M5980</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-07-16T21:11:58Z</dc:date>
    </item>
  </channel>
</rss>