<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>NFC中的主题 PN7462 RF field on problem</title>
    <link>https://community.nxp.com/t5/NFC/PN7462-RF-field-on-problem/m-p/932568#M5756</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PN7462 custom board, problem with RF field on with NFC Cockpit. I designed my own board with PN7462. It based on development kit OM27462CDK. My schematic is in attachment. I have som FW to EVB when board is login into windows as COM port. this same FW I flashed to my board. When I tried to turn on RF field i gave erro message that RF field cannot be turn on. But on oscilloscope I measured that field is on. In my schematic if i desoldered B4 than i dont have problem but of course when i tried measure field was off. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Jul 2019 06:38:54 GMT</pubDate>
    <dc:creator>cepec</dc:creator>
    <dc:date>2019-07-31T06:38:54Z</dc:date>
    <item>
      <title>PN7462 RF field on problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-RF-field-on-problem/m-p/932568#M5756</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PN7462 custom board, problem with RF field on with NFC Cockpit. I designed my own board with PN7462. It based on development kit OM27462CDK. My schematic is in attachment. I have som FW to EVB when board is login into windows as COM port. this same FW I flashed to my board. When I tried to turn on RF field i gave erro message that RF field cannot be turn on. But on oscilloscope I measured that field is on. In my schematic if i desoldered B4 than i dont have problem but of course when i tried measure field was off. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 06:38:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-RF-field-on-problem/m-p/932568#M5756</guid>
      <dc:creator>cepec</dc:creator>
      <dc:date>2019-07-31T06:38:54Z</dc:date>
    </item>
    <item>
      <title>Re: PN7462 RF field on problem</title>
      <link>https://community.nxp.com/t5/NFC/PN7462-RF-field-on-problem/m-p/932569#M5757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looks like the connection of TVDD_OUT is different from the EVB, Please refer to the following for details.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/84575i4F1DC2D6C71CCD40/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please try to remove B3 on your board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 03:16:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/NFC/PN7462-RF-field-on-problem/m-p/932569#M5757</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-08-01T03:16:32Z</dc:date>
    </item>
  </channel>
</rss>